Part Number: AM4378
Hi,
I'm considering using AM437x's Linux SDK for development.
Q1.
Can IPv6 communication be performed using the AM437x processor?
As far as TRM is concerned, it seems to support IPv6.
Q2.
When using the IPv6 DHCP client function, which of the following protocols is supported?
・RA (Router Advertisements)
・Stateless DHCPv6
・Stateful DHCPv6
Q3.
In a network environment where both IPv4 and IPv6 can be used, is it possible to select which protocol to use for communication? Are there any priorities?
Thanks,
Eevee