This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: how to enable High Security on GP device?

Part Number: TDA4VM

My TDA4 chip number is  TDA4VM88TGBALFRQ1,and the chip on evaluation board is XJ721EGBALF.

they are both GENERAL PURPOSE (GP) Device type, that's right?

my question is: Can I enable High Security on these GP devices?

  • Hi,

    Can you describe what security features you need to n GP samples? The ROM code on GP devices does not authenticate any image.

    Regards,

    Keerthy

  • so if I want to enable security features, i must buy the HS device type chip?

    according to the doc:Security Enablers on JacintoTm 7 Processors

    on TDA4VM TI can enable 12 security features, so which one can i enable on GP devices?

    Device identity (unique ID).

    Secure boot (root-of-trust public key).

    Initial secure programming.

    Cryptographic acceleration.

    External memory protection (firewalls).

    Debugging security (Joint Test Action Group [JTAG] lock with password).

    Software intellectual property (IP) protection (debugging lockout).

    • Secure Storage

    • Physical security

    • Network security

    • Secure firmware and software update

    • Trusted Executable Environment