This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: AM62x family(am625): TI am625 machine failed

Part Number: AM625

Hi Expert!

Facing below issue.

ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/recipe-sysroot-native/lib -Wl,-rpath,/home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/recipe-sysroot-native/usr/lib -Wl,-rpath,/home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/recipe-sysroot-native/lib -Wl,-O1 -Wl,--allow-shlib-undefined -Wl,--dynamic-linker=/home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/sysroots-uninative/x86_64-linux/lib/ld-linux-x86-64.so.2 -o scripts/kconfig/conf scripts/kconfig/conf.o scripts/kconfig/zconf.tab.o
| scripts/kconfig/conf --defconfig=arch/../configs/am62x_evm_r5_defconfig Kconfig
| ***
| *** Can't find default configuration "arch/../configs/am62x_evm_r5_defconfig"!
| ***
| /home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/git/scripts/kconfig/Makefile:128: recipe for target 'am62x_evm_r5_defconfig' failed
| make[2]: *** [am62x_evm_r5_defconfig] Error 1
| /home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/git/Makefile:539: recipe for target 'am62x_evm_r5_defconfig' failed
| make[1]: *** [am62x_evm_r5_defconfig] Error 2
| make[1]: Leaving directory '/home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/build'
| Makefile:167: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2
| make: Leaving directory '/home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/git'
| ERROR: oe_runmake failed
| WARNING: /home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/temp/run.do_configure.30346:1 exit 1 from 'exit 1'
| ERROR: Execution of '/home/aws-suma/OneControl/build-lrd-am62xx-onecontrol-lrd-5.10-rt-test/tmp/work/am62xx_onecontrol_lrd_k3r5_hs_se-poky-linux-gnueabi/u-boot-ti-staging/1_2020.01+gitAUTOINC+2781231a33-r36/temp/run.do_configure.30346' failed with exit code 1
ERROR: Task (mc:k3r5-hs-se:/home/aws-suma/OneControl/yocto/meta-ti/recipes-bsp/u-boot/u-boot-ti-staging_2020.01.bb:do_configure) failed with exit code '1'

Is there any ti related changes happned ? for hs-se machine ?

Thanks,

Suraj.