This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: default norflash read/write failed with the default source code of v8.6

Part Number: TDA4VM
Other Parts Discussed in Thread: TDA4VH

Have build psdkla v8.6 for VH, have found that the default source code of s28hs512t could not read/write data. Could you provide patches for this problem? Great thanks!

Log showed as below:

[    1.222918] cadence-qspi 47040000.spi: error -ENODEV: No Rx DMA available
[    1.230397] spi-nor spi1.0: Software reset done, line 3405
[    1.235906] NOR: name:s25sl032p read_id ok
[    1.240450] spi-nor spi1.0: s28hs512t (65536 Kbytes)
[    1.245416] 7 cmdlinepart partitions found on MTD device 47040000.spi.0
[    1.252014] Creating 7 MTD partitions on "47040000.spi.0":
[    1.257488] 0x000000000000-0x000000080000 : "ospi.tiboot3"
[    1.263571] 0x000000080000-0x000000280000 : "ospi.tispl"
[    1.269371] 0x000000280000-0x000000680000 : "ospi.u-boot"
[    1.275244] 0x000000680000-0x0000006c0000 : "ospi.env"
[    1.280849] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
[    1.287061] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
[    1.292934] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
[    1.299145] NOR: spi_nor_probe done

~# flashcp phy /dev/mtd0 -v
Erasing blocks: 1/1 (100%)
While erasing blocks 0x00000000-0x00040000 on /dev/mtd0: Invalid argument

  • Hi,

    Couple of questions.

    • Is this a custom board? Or TI EVM?
    • Was it working in the previous SDK versions?
    • Can you please share the complete boot logs from SPL?

    Best Regards,

    Keerthy

  • Hi,

    • Is this a custom board? Or TI EVM?

    custom board, but the same hardware ref design with ti EVM.

    • Was it working in the previous SDK versions?

    NO, could read device id correctly only.

    • Can you please share the complete boot logs from SPL?

    Please found the detail below.

    U-Boot SPL 2021.01-dirty (Mar 21 2023 - 10:46:10 +0800)
    EEPROM not available at 0x50, trying to read at 0x51
    Reading on-board EEPROM at 0x51 failed 1
    SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    SPL initial stack usage: 13472 bytes
    Trying to boot from MMC2
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
    NOTICE:  BL31: Built : 15:42:56, Mar 13 2023
    I/TC:
    I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Mon Mar 13 15:43:08 UTC 2023 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    I/TC: HUK Initialized
    I/TC: Activated SA2UL device
    I/TC: Fixing SA2UL firewall owner for GP device
    I/TC: Enabled firewalls for SA2UL TRNG device
    I/TC: SA2UL TRNG initialized
    I/TC: SA2UL Drivers initialized
    I/TC: Primary CPU switching to normal world boot
    
    U-Boot SPL 2021.01-dirty (Mar 21 2023 - 10:45:54 +0800)
    SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    Trying to boot from MMC2
    
    
    U-Boot 2021.01-dirty (Mar 21 2023 - 10:45:54 +0800)
    
    SoC:   J784S4 SR1.0 GP
    Model: Texas Instruments J784S4 EVM
    EEPROM not available at 0x50, trying to read at 0x51
    Reading on-board EEPROM at 0x51 failed 1
    Board: J784S4-EVM rev E1
    DRAM:  32 GiB
    idle-statesFlash: 0 Bytes
    MMC:   mmc@4f80000: 0, mmc@4fb0000: 1
    Loading Environment from MMC... OK
    In:    serial@2880000
    Out:   serial@2880000
    Err:   serial@2880000
    am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
    EEPROM not available at 0x50, trying to read at 0x51
    Reading on-board EEPROM at 0x51 failed 1
    Net:   Could not get PHY for ethernet@46000000port@1: addr 0
    am65_cpsw_nuss_port ethernet@46000000port@1: phy_connect() failed
    No ethernet found.
    
    Hit any key to stop autoboot:  0
    pca953x gpio@22: Error reading output register
    switch to partitions #0, OK
    mmc1 is current device
    pca953x gpio@22: Error reading output register
    SD/MMC found on device 1
    Failed to load 'boot.scr'
    484 bytes read in 10 ms (46.9 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    Running uenvcmd ...
    1 bytes read in 11 ms (0 Bytes/s)
    Already setup.
    pca953x gpio@20: Error reading output register
    GPIO: 'gpio@22_17' not found
    Command 'gpio' failed: Error -121
    pca953x gpio@20: Error reading output register
    GPIO: 'gpio@22_16' not found
    Command 'gpio' failed: Error -121
    pca953x gpio@20: Error reading output register
    GPIO: 'gpio@22_13' not found
    Command 'gpio' failed: Error -121
    pca953x gpio@20: Error reading output register
    GPIO: 'gpio@22_14' not found
    Command 'gpio' failed: Error -121
    pca953x gpio@20: Error reading output register
    GPIO: 'gpio@22_15' not found
    Command 'gpio' failed: Error -121
    k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
    k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
    1428772 bytes read in 71 ms (19.2 MiB/s)
    Load Remote Processor 2 with data@addr=0x82000000 1428772 bytes: Success!
    301996 bytes read in 25 ms (11.5 MiB/s)
    Load Remote Processor 3 with data@addr=0x82000000 301996 bytes: Success!
    179128 bytes read in 20 ms (8.5 MiB/s)
    Load Remote Processor 4 with data@addr=0x82000000 179128 bytes: Success!
    179128 bytes read in 20 ms (8.5 MiB/s)
    Load Remote Processor 5 with data@addr=0x82000000 179128 bytes: Success!
    596856 bytes read in 37 ms (15.4 MiB/s)
    Load Remote Processor 6 with data@addr=0x82000000 596856 bytes: Success!
    179128 bytes read in 20 ms (8.5 MiB/s)
    Load Remote Processor 7 with data@addr=0x82000000 179128 bytes: Success!
    14684456 bytes read in 618 ms (22.7 MiB/s)
    Load Remote Processor 8 with data@addr=0x82000000 14684456 bytes: Success!
    14946600 bytes read in 629 ms (22.7 MiB/s)
    Load Remote Processor 9 with data@addr=0x82000000 14946600 bytes: Success!
    14553384 bytes read in 613 ms (22.6 MiB/s)
    Load Remote Processor 10 with data@addr=0x82000000 14553384 bytes: Success!
    14553384 bytes read in 613 ms (22.6 MiB/s)
    Load Remote Processor 11 with data@addr=0x82000000 14553384 bytes: Success!
    19079680 bytes read in 793 ms (22.9 MiB/s)
    99957 bytes read in 14 ms (6.8 MiB/s)
    14313 bytes read in 11 ms (1.2 MiB/s)
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
       Loading Device Tree to 000000008fee4000, end 000000008fffffff ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
    [    0.000000] Linux version 5.10.162-g76b3e88d56 (ubuntu@ubuntu) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (a-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #2 SMP PREEMPT Tue Mar 21 17:22:35 C 2023
    [    0.000000] Machine model: Texas Instruments J784S4 EVM
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002880000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a8000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a8100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@aa000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000aa100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@aa100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 48 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-rtos-ipc-memory-region@ac000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000af000000, size 80 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@af000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b4000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b4000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b4100000, size 51 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@b4100000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b7400000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@b7400000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b7500000, size 51 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@b7500000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ba800000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_2-dma-memory@ba800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ba900000, size 51 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_2-memory@ba900000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000bdc00000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_3-dma-memory@bdc00000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000bdd00000, size 51 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_3-memory@bdd00000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000e1000000, size 80 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@e1000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000e6000000, size 8 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-queues@e6000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000e6800000, size 24 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-virtual-eth-buffers@e6800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 2048 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000900000000, size 1792 MiB
    [    0.000000] OF: reserved mem: initialized node linux-cma-buffers@900000000, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x0000000fffffefff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x00000000c0ffffff]
    [    0.000000]   node   0: [mem 0x00000000c1000000-0x00000000e0ffffff]
    [    0.000000]   node   0: [mem 0x00000000e1000000-0x00000000e7ffffff]
    [    0.000000]   node   0: [mem 0x00000000e8000000-0x00000000ffffefff]
    [    0.000000]   node   0: [mem 0x0000000880000000-0x00000008ffffffff]
    [    0.000000]   node   0: [mem 0x0000000900000000-0x0000000fffffefff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x0000000fffffefff]
    [    0.000000] On node 0, zone Normal: 1 pages in unavailable ranges
    [    0.000000] On node 0, zone Normal: 1 pages in unavailable ranges
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.2
    [    0.000000] percpu: Embedded 22 pages/cpu s50392 r8192 d31528 u90112
    [    0.000000] Detected PIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: EL2 vector hardening
    [    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
    [    0.000000] CPU features: detected: Spectre-BHB
    [    0.000000] CPU features: detected: ARM erratum 1742098
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 8257534
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02880000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc-boot),256k(hbmc.env),-@8m(hbmc.rootfs) root=PARTUUID=d17d6e24-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 4194304 (order: 13, 33554432 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 2097152 (order: 12, 16777216 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
    [    0.000000] Memory: 27698048K/33554424K available (11200K kernel code, 1160K rwdata, 4300K rodata, 1856K init, 433K bss, 4021368K reserved, 1835008K cmreserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=8, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=8.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000]  Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=8
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 960 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] GICv3: Distributor has no Range Selector support
    [    0.000000] GICv3: 16 PPIs implemented
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @970800000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x0000000970050000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000970060000
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000001] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008433] Console: colour dummy device 80x25
    [    0.012999] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023669] pid_max: default: 32768 minimum: 301
    [    0.028433] LSM: Security Framework initializing
    [    0.033335] Mount-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.041225] Mountpoint-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.050384] rcu: Hierarchical SRCU implementation.
    [    0.055431] Platform MSI: msi-controller@1820000 domain created
    [    0.061627] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.070932] EFI services will not be available.
    [    0.075784] smp: Bringing up secondary CPUs ...
    I/TC: Secondary CPU 1 initializing
    I/TC: Secondary CPU 1 switching to normal world boot
    I/TC: Secondary CPU 2 initializing
    I/TC: Secondary CPU 2 switching to normal world boot
    I/TC: Secondary CPU 3 initializing
    I/TC: Secondary CPU 3 switching to normal world boot
    I/TC: Secondary CPU 2 initializing
    I/TC: Secondary CPU 2 switching to normal world boot
    I/TC: Secondary CPU 3 initializing
    I/TC: Secondary CPU 3 switching to normal world boot
    I/TC: Secondary CPU 4 initializing
    I/TC: Secondary CPU 4 switching to normal world boot
    I/TC: Secondary CPU 5 initializing
    I/TC: Secondary CPU 5 switching to normal world boot
    [    0.088857] Detected PIPT I-cache on CPU1
    [    0.088881] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
    [    0.088893] GICv3: CPU1: using allocated LPI pending table @0x0000000970070000
    [    0.088929] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
    [    0.097366] Detected PIPT I-cache on CPU2
    [    0.097380] GICv3: CPU2: found redistributor 2 region 0:0x0000000001940000
    [    0.097391] GICv3: CPU2: using allocated LPI pending table @0x0000000970080000
    [    0.097419] CPU2: Booted secondary processor 0x0000000002 [0x411fd080]
    [    0.105838] Detected PIPT I-cache on CPU3
    [    0.105854] GICv3: CPU3: found redistributor 3 region 0:0x0000000001960000
    [    0.105866] GICv3: CPU3: using allocated LPI pending table @0x0000000970090000
    [    0.105893] CPU3: Booted secondary processor 0x0000000003 [0x411fd080]
    [    0.114344] Detected PIPT I-cache on CPU4
    [    0.114370] GICv3: CPU4: found redistributor 100 region 0:0x0000000001980000
    [    0.114383] GICv3: CPU4: using allocated LPI pending table @0x00000009700a0000
    [    0.114419] CPU4: Booted secondary processor 0x0000000100 [0x411fd080]
    [    0.122884] Detected PIPT I-cache on CPU5
    [    0.122903] GICv3: CPU5: found redistributor 101 region 0:0x00000000019a0000
    [    0.122914] GICv3: CPU5: using allocated LPI pending table @0x00000009700b0000
    [    0.122942] CPU5: Booted secondary processor 0x0000000101 [0x411fd080]
    [    0.131372] Detected PIPT I-cache on CPU6
    [    0.131392] GICv3: CPU6: found redistributor 102 region 0:0x00000000019c0000
    [    0.131403] GICv3: CPU6: using allocated LPI pending table @0x00000009700c0000
    [    0.131431] CPU6: Booted secondary processor 0x0000000102 [0x411fd080]
    [    0.139848] Detected PIPT I-cache on CPU7
    [    0.139869] GICv3: CPU7: found redistributor 103 region 0:0x00000000019e0000
    [    0.139880] GICv3: CPU7: using allocated LPI pending table @0x00000009700d0000
    [    0.139908] CPU7: Booted secondary processor 0x0000000103 [0x411fd080]
    [    0.139960] smp: Brought up 1 node, 8 CPUs
    [    0.320945] SMP: Total of 8 processors activated.
    [    0.325751] CPU features: detected: 32-bit EL0 Support
    [    0.331006] CPU features: detected: CRC32 instructions
    [    0.347543] CPU: All CPU(s) started at EL2
    [    0.351749] alternatives: patching kernel code
    [    0.356937] devtmpfs: initialized
    [    0.365445] KASLR disabled due to lack of seed
    [    0.370083] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.380049] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
    [    0.405382] pinctrl core: initialized pinctrl subsystem
    [    0.411056] DMI not present or invalid.
    [    0.415315] NET: Registered protocol family 16
    [    0.421298] DMA: preallocated 4096 KiB GFP_KERNEL pool for atomic allocations
    [    0.429302] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.438011] DMA: preallocated 4096 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.446460] thermal_sys: Registered thermal governor 'step_wise'
    [    0.446463] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.453059] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.466756] ASID allocator initialised with 65536 entries
    [    0.484063] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.490919] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.497767] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.504614] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.512123] cryptd: max_cpu_qlen set to 1000
    [    0.518167] k3-chipinfo 43000014.chipid: Family:J784S4 rev:SR1.0 JTAGID[0x0bb8002f] Detected
    [    0.527042] vsys_3v3: supplied by evm_12v0
    [    0.531417] vsys_5v0: supplied by evm_12v0
    [    0.536235] iommu: Default domain type: Translated
    [    0.541348] SCSI subsystem initialized
    [    0.545308] mc: Linux media interface: v0.10
    [    0.549678] videodev: Linux video capture interface: v2.00
    [    0.555306] pps_core: LinuxPPS API ver. 1 registered
    [    0.560377] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.569715] PTP clock support registered
    [    0.573736] EDAC MC: Ver: 3.0.0
    [    0.577462] FPGA manager framework
    [    0.580970] Advanced Linux Sound Architecture Driver Initialized.
    [    0.587586] clocksource: Switched to clocksource arch_sys_counter
    [    0.593897] VFS: Disk quotas dquot_6.6.0
    [    0.597931] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.607637] Carveout Heap: Exported 512 MiB at 0x00000000c1000000
    [    0.613914] NET: Registered protocol family 2
    [    0.619123] IP idents hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.630083] tcp_listen_portaddr_hash hash table entries: 16384 (order: 6, 262144 bytes, linear)
    [    0.639182] TCP established hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.648264] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes, linear)
    [    0.656259] TCP: Hash tables configured (established 262144 bind 65536)
    [    0.663155] UDP hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.670491] UDP-Lite hash table entries: 16384 (order: 7, 524288 bytes, linear)
    [    0.678344] NET: Registered protocol family 1
    [    0.683171] RPC: Registered named UNIX socket transport module.
    [    0.689235] RPC: Registered udp transport module.
    [    0.694041] RPC: Registered tcp transport module.
    [    0.698846] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.705431] NET: Registered protocol family 44
    [    0.709978] PCI: CLS 0 bytes, default 64
    [    0.714645] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
    [    0.725292] Initialise system trusted keyrings
    [    0.729928] workingset: timestamp_bits=46 max_order=23 bucket_order=0
    [    0.738099] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.744272] NFS: Registering the id_resolver key type
    [    0.749448] Key type id_resolver registered
    [    0.753721] Key type id_legacy registered
    [    0.757840] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.764688] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.772306] 9p: Installing v9fs 9p2000 file system support
    [    0.797295] Key type asymmetric registered
    [    0.801483] Asymmetric key parser 'x509' registered
    [    0.806479] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
    [    0.814043] io scheduler mq-deadline registered
    [    0.818670] io scheduler kyber registered
    [    0.824172] pinctrl-single 4301c000.pinctrl: 101 pins, size 404
    [    0.830355] pinctrl-single 11c000.pinctrl: 72 pins, size 288
    [    0.840147] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    0.852671] brd: module loaded
    [    0.859535] loop: module loaded
    [    0.863216] megasas: 07.714.04.00-rc1
    [    0.868604] tun: Universal TUN/TAP device driver, 1.6
    [    0.873993] igbvf: Intel(R) Gigabit Virtual Function Network Driver
    [    0.880399] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
    [    0.886466] sky2: driver version 1.30
    [    0.890567] VFIO - User Level meta-driver version: 0.3
    [    0.896248] i2c /dev entries driver
    [    0.900518] sdhci: Secure Digital Host Controller Interface driver
    [    0.906834] sdhci: Copyright(c) Pierre Ossman
    [    0.911441] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.917792] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.924080] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.931320] optee: probing for conduit method.
    I/TC: Reserved shared memory is enabled
    I/TC: Dynamic shared memory is enabled
    I/TC: Normal World virtualization support is disabled
    I/TC: Asynchronous notifications are disabled
    [    0.935877] optee: revision 3.20 (8e74d476)
    [    0.952265] optee: dynamic shared memory is enabled
    [    0.961730] optee: initialized driver
    [    0.966484] NET: Registered protocol family 17
    [    0.971094] 9pnet: Installing 9P2000 support
    [    0.975485] Key type dns_resolver registered
    [    0.979960] Loading compiled-in X.509 certificates
    [    0.990400] ti-sci 44083000.system-controller: ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
    [    1.019787] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 177 domain created
    [    1.028332] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 10 domain created
    [    1.037585] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 283 domain created
    [    1.046228] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 321 created
    [    1.057736] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
    [    1.065405] j721e-pcie 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
    [    1.073688] j721e-pcie 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
    [    1.081969] j721e-pcie 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    1.090766] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    1.098429] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    1.106705] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    1.114982] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    1.123884] ti-udma 311a0000.dma-controller: Number of rings: 48
    [    1.130671] ti-udma 311a0000.dma-controller: Channels: 24 (bchan: 0, tchan: 8, rchan: 16)
    [    1.139831] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:328
    [    1.149702] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
    [    1.156461] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
    [    1.165324] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[878,128] sci-dev-id:315
    [    1.175467] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
    [    1.182226] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
    [    1.190101] printk: console [ttyS2] disabled
    [    1.194491] 2880000.serial: ttyS2 at MMIO 0x2880000 (irq = 17, base_baud = 3000000) is a 8250
    [    1.203239] printk: console [ttyS2] enabled
    [    1.203239] printk: console [ttyS2] enabled
    [    1.211675] printk: bootconsole [ns16550a0] disabled
    [    1.211675] printk: bootconsole [ns16550a0] disabled
    [    1.222918] cadence-qspi 47040000.spi: error -ENODEV: No Rx DMA available
    [    1.230397] spi-nor spi1.0: Software reset done, line 3405
    [    1.235906] NOR: name:s25sl032p read_id ok
    [    1.240450] spi-nor spi1.0: s28hs512t (65536 Kbytes)
    [    1.245416] 7 cmdlinepart partitions found on MTD device 47040000.spi.0
    [    1.252014] Creating 7 MTD partitions on "47040000.spi.0":
    [    1.257488] 0x000000000000-0x000000080000 : "ospi.tiboot3"
    [    1.263571] 0x000000080000-0x000000280000 : "ospi.tispl"
    [    1.269371] 0x000000280000-0x000000680000 : "ospi.u-boot"
    [    1.275244] 0x000000680000-0x0000006c0000 : "ospi.env"
    [    1.280849] 0x0000006c0000-0x000000700000 : "ospi.env.backup"
    [    1.287061] 0x000000800000-0x000003fc0000 : "ospi.rootfs"
    [    1.292934] 0x000003fc0000-0x000004000000 : "ospi.phypattern"
    [    1.299145] NOR: spi_nor_probe done
    [    1.405070] mmc0: CQHCI version 5.10
    [    1.405271] mmc1: CQHCI version 5.10
    [    1.415488] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fca100
    [    1.422305] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fca100
    [    1.429107] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fca100
    [    1.435904] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fca100
    [    1.442704] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fca100
    [    1.449503] omap-mailbox 31f85000.mailbox: omap mailbox rev 0x66fca100
    [    1.449538] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
    [    1.449546] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
    [    1.503363] mmc1: new SDHC card at address aaaa
    [    1.508224] mmcblk1: mmc1:aaaa SD32G 29.7 GiB
    [    1.514171]  mmcblk1: p1 p2
    [    1.523974] mmc0: mmc_select_hs200 failed, error -110
    [    1.529023] mmc0: error -110 whilst initialising MMC card
    [    1.657532] mmc0: mmc_select_hs200 failed, error -110
    [    1.662573] mmc0: error -110 whilst initialising MMC card
    [    1.804857] mmc0: mmc_select_hs200 failed, error -110
    [    1.809899] mmc0: error -110 whilst initialising MMC card
    [    1.994428] mmc0: mmc_select_hs200 failed, error -110
    [    1.999473] mmc0: error -110 whilst initialising MMC card
    [    2.171994] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
    [    2.179473] j721e-pcie 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
    [    2.187555] j721e-pcie 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
    [    2.195640] j721e-pcie 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    2.204240] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    2.211728] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    2.219807] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    2.227887] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    2.236846] ti-udma 285c0000.dma-controller: Channels: 22 (tchan: 11, rchan: 11, gp-rflow: 8)
    [    2.246784] ti-udma 31150000.dma-controller: Channels: 66 (tchan: 33, rchan: 33, gp-rflow: 16)
    [    2.257342] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
    [    2.264826] j721e-pcie 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
    [    2.272907] j721e-pcie 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
    [    2.280987] j721e-pcie 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    2.289507] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    2.296996] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    2.305074] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    2.313156] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    2.322223] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
    [    2.329703] j721e-pcie 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
    [    2.337785] j721e-pcie 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
    [    2.345866] j721e-pcie 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    2.354381] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
    [    2.361861] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
    [    2.369940] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
    [    2.378019] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
    [    2.386563] debugfs: Directory 'pd:74' with parent 'pm_genpd' already present!
    [    2.393789] debugfs: Directory 'pd:73' with parent 'pm_genpd' already present!
    [    2.401075] debugfs: Directory 'pd:72' with parent 'pm_genpd' already present!
    [    2.408726] debugfs: Directory 'pd:335' with parent 'pm_genpd' already present!
    [    2.416053] debugfs: Directory 'pd:333' with parent 'pm_genpd' already present!
    [    2.423365] debugfs: Directory 'pd:332' with parent 'pm_genpd' already present!
    [    2.436646] ALSA device list:
    [    2.439610]   No soundcards found.
    [    2.467315] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
    [    2.475433] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    2.494169] devtmpfs: mounted
    [    2.497819] Freeing unused kernel memory: 1856K
    [    2.502451] Run /sbin/init as init process
    [    3.111732] systemd[1]: System time before build time, advancing clock.
    [    3.213097] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUT +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    3.234921] systemd[1]: Detected architecture arm64.
    
    Welcome to Arago 2021.09!
    
    [    3.280477] systemd[1]: Set hostname to <j784s4-evm>.
    [    3.559081] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
    [    3.567971] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
    [    3.582233] systemd[1]: /lib/systemd/system/irqbalanced.service:6: Unknown key name 'ConditionCPUs' in section 'Unit', ignoring.
    [    3.607056] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/dockerock → /run/docker.sock; please update the unit file accordingly.
    [    3.683473] random: systemd: uninitialized urandom read (16 bytes read)
    [    3.691707] systemd[1]: Created slice system-getty.slice.
    [  OK  ] Created slice system-getty.slice.
    [    3.711704] random: systemd: uninitialized urandom read (16 bytes read)
    [    3.719119] systemd[1]: Created slice system-serial\x2dgetty.slice.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    3.739643] random: systemd: uninitialized urandom read (16 bytes read)
    [    3.746874] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    3.767750] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password …ts to Console Directory Watch.
    [    3.791689] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password R…uests to Wall Directory Watch.
    [    3.815696] systemd[1]: Reached target Paths.
    [  OK  ] Reached target Paths.
    [    3.835641] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    3.855633] systemd[1]: Reached target Slices.
    [  OK  ] Reached target Slices.
    [    3.875640] systemd[1]: Reached target Swap.
    [  OK  ] Reached target Swap.
    [    3.913227] systemd[1]: Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [    3.935758] systemd[1]: Reached target RPC Port Mapper.
    [  OK  ] Reached target RPC Port Mapper.
    [    3.962391] systemd[1]: Listening on Process Core Dump Socket.
    [  OK  ] Listening on Process Core Dump Socket.
    [    3.983744] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    4.009085] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
    [    4.017341] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    4.039831] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    4.055842] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    4.079776] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    4.099728] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    4.121635] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    4.137591] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    4.161464] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    4.178564] systemd[1]: Mounting Temporary Directory (/tmp)...
             Mounting Temporary Directory (/tmp)...
    [    4.195780] systemd[1]: Condition check resulted in Create list of static device nodes for the current kernel being skipped.
    [    4.223048] systemd[1]: Starting Start psplash boot splash screen...
             Starting Start psplash boot splash screen...
    [    4.249992] systemd[1]: Starting RPC Bind...
             Starting RPC Bind...
    [    4.267853] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
    [    4.279715] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.343740] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.365894] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
    [0m...
    [    4.401913] systemd[1]: Starting udev Coldplug all Devices...
             Starting udev Coldplug all Devices...
    [    4.426293] systemd[1]: Started RPC Bind.
    [  OK  ] Started RPC Bind.
    [    4.439805] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted Huge Pages File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory (/tmp).
    [FAILED] Failed to start Start psplash boot splash screen.
    See 'systemctl status psplash-start.service' for details.
    [DEPEND] Dependency failed for Star…progress communication helper.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Started Remount Root and Kernel File Systems.
             Mounting Kernel Configuration File System...
             Starting Flush Journal to Persistent Storage...
    [    4.670684] systemd-journald[193]: Received client request to flush runtime journal.
             Starting Apply Kernel Variables...
    [    4.695869] random: systemd: uninitialized urandom read (16 bytes read)
             Starting Create Static Device Nodes in /dev    4.705461] random: systemd-journal: uninitialized urandom read (16 bytes read)
    m...
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started udev Coldplug all Devices.
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [    4.828033] random: systemd: uninitialized urandom read (16 bytes read)
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /media/ram...
             Mounting /var/volatile...
             Starting udev Wait for Complete Device Initialization...
             Starting udev Kernel Device Manager...
    [  OK  ] Mounted /media/ram.
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Network Time Synchronization...
             Starting Update UTMP about System Boot/Shutdown...
    [  OK  ] Started udev Kernel Device Manager.
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Set.
    [  OK  ] Reached target System Time Synchronized.
    [    5.729631] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.736321] random: systemd: uninitialized urandom read (16 bytes read)
    [    5.742962] random: systemd: uninitialized urandom read (16 bytes read)
    [  OK  ] Created slice system-systemd\x2dfsck.slice.
    [  OK  ] Found device /dev/mmcblk1p1.
    [  OK  ] Started udev Wait for Complete Device Initialization.
    [  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily rotation of log files.
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
             Starting Docker Socket for the API.
    [  OK  ] Listening on dropbear.socket.
             Starting Reboot and dump vmcore via kexec...
             Starting File System Check on /dev/mmcblk1p1...
    [  OK  ] Listening on Docker Socket for the API.
    [  OK  ] Started Reboot and dump vmcore via kexec.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
    [  OK  ] Started Job spooling tools.
    [  OK  ] Started Periodic Command Scheduler.
    [  OK  ] Started D-Bus System Message Bus.
             Starting Print notice about GPLv3 packages...
             Starting set host name as per compatible name...
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
    [  OK  ] Started irqbalance daemon.
             Starting Telephony service...
             Starting rc.pvr.service...
             Starting Login Service...
    [  OK  ] Started TEE Supplicant.
             Starting Update weston ini… based on the platform name...
    [    6.811597] random: crng init done
    [    6.814995] random: 219 urandom warning(s) missed due to ratelimiting
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started File System Check on /dev/mmcblk1p1.
    [  OK  ] Started set host name as per compatible name.
    [  OK  ] Started IPv6 Packet Filtering Framework.
    [  OK  ] Started IPv4 Packet Filtering Framework.
    [  OK  ] Started rc.pvr.service.
    [  OK  ] Started Update weston ini …ge based on the platform name.
    [  OK  ] Started Telephony service.
    [  OK  ] Reached target Network (Pre).
             Mounting /run/media/mmcblk1p1...
             Starting Network Service...
             Starting weston.service...
    [  OK  ] Started Login Service.
    [  OK  ] Mounted /run/media/mmcblk1p1.
    [  OK  ] Started Network Service.
             Starting Wait for Network to be Configured...
             Starting Network Name Resolution...
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Reached target Network.
    [  OK  ] Reached target Host and Network Name Lookups.
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Enable and configure wl18xx bluetooth stack...
    [  OK  ] Started NFS status monitor for NFSv2/3 locking..
             Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
             Starting Permit User Sessions...
    [  OK  ] Started Enable and configure wl18xx bluetooth stack.
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Login Prompts.
             Starting Synchronize System and HW clocks...
    [FAILED] Failed to start Synchronize System and HW clocks.
    See 'systemctl status sync-clocks.service' for details.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Started Simple Network Man…ement Protocol (SNMP) Daemon..
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPLv3 packages:
            autoconf
            bash-dev
            bash
            bc
            binutils
            cifs-utils
            coreutils-stdbuf
            coreutils
            cpio
            cpp-symlinks
            cpp
            dosfstools
            elfutils
            g++-symlinks
            g++
            gawk
            gcc-symlinks
            gcc
            gdb
            gdbserver
            gettext
            glmark2
            gstreamer1.0-libav-dev
            gstreamer1.0-libav
            gzip
            less
            libasm1
            libbfd
            libdw1
            libelf1
            libgdbm-compat4
            libgdbm-dev
            libgdbm6
            libgettextlib
            libgettextsrc
            libgmp-dev
            libgmp10
            libgmpxx4
            libidn2-0
            libidn2-dev
            libmpc3
            libmpfr6
            libreadline-dev
            libreadline8
            libunistring-dev
            libunistring2
            m4-dev
            m4
            make
            nettle-dev
            nettle
            parted
            python3-rfc3987
            python3-strict-rfc3339
            tar
            which
            zeromq
    
    If you do not wish to distribute GPLv3 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above
    
    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
    [  OK  ] Started Print notice about GPLv3 packages.
    [  OK  ] Started weston.service.
             Starting DEMO...
             Starting EdgeAI OOB demos...
             Starting telnetd.service...
    [  OK  ] Started DEMO.
    [  OK  ] Started telnetd.service.
    
     _____                    _____           _         _
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
                  |___|                    |___|
    
    Arago Project j784s4-evm ttyS2
    
    Arago 2021.09 j784s4-evm ttyS2
    
    j784s4-evm login: root
    

  • Could you kindly check and provide some patches ? Great thanks!

    • Was it working in the previous SDK versions?

    NO, could read device id correctly only.

    Before v8.6, the "# CONFIG_MTD_SPI_NAND is not set";

    with v8.6, "CONFIG_MTD_SPI_NAND=y" set defaultly.

  • Hi,

    I got a confirmation from my internal team that 8.6 does NOT support NAND on TDA4VH from Linux kernel.
    It is enabled for a different SoC & hence the config is set.

    - Keerthy

  • Thanks for your reply!

    We have found below error during system bootup, it seems like the cadence-qspi device have probed failed.And this error have not found on v8.5.

    Could you provide patch for this error ?

    [    1.222918] cadence-qspi 47040000.spi: error -ENODEV: No Rx DMA available

  • Hi,

    Please create a different thread with the compete logs. Closing this one.

    - Keerthy