Part Number: TDA4VM
Hi,
I am trying to bring up the new TDA4VM Starter kit we have received yesterday.
Using the USB serial connection It is clear that the bootup starts but freezes at this line:
1334036 bytes read in 66 ms (19.3 MiB/s) Load Remote Processor 6 with data@addr=0x82000000 1334036 bytes: Success! 1334036 bytes read in 67 ms (19 MiB/s) Load
There is no device connected to the SoC, only the power and the micro-USB.
These are the steps I already tried:
1. First I tried to build the SD card using the latest SDK 8.6 by building all the components.
2. Building SD card using the image provided:
https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-SK-TDA4VM/08.06.00.11
3. Building SD card using the previous version 8.5
I haven't changed any of the configurations, just used the image as-is.
Please check the provided log attached.
Michael