Part Number: PROCESSOR-SDK-J721E
[Note: words underlined and blue are links to relevant sites]
We’re trying to reproduce the steps for generating a QNX sd card image for the board j721e_evm but, even though we met the QNX SDP software dependencies, the build step make qnx_fs_create returns the following error because of a missing graphical library:

Seems like a folder /usr/lib/graphics/j721e/ is missing.
Currently we have available in the folder /qnx710/target/qnx7/aarch64le/usr/lib/graphics the following folders:
- Dummy
- Dummy-debug
- Jacinto7
- Jacinto7-debug
- Vulkan
Searching for similarities we’ve found in QNX software center this package, which contains a folder called /usr/lib/graphics/j721s2/ (very similar to the one needed):

These are the packages that we have currently installed:
Our question is:
- Is there any similar package called com.qnx.qnx710.target.screen.board.j721e or any possibility of building the sd card image without graphical libraries?
Antonio