Part Number: SK-TDA4VM
I am using the J721s2 SoC board with the TDA4 common processor board and an attached fusion application board. I have successfully built the vision apps (with PROFILE=release) using the j721s2 RTOS PSDK, and am able to run the single camera application with an AR0233 sensor. Linux console output from the A72 cores shows up as expected on the lowest COM port associated with J44, but I am seeing no output on any of the other COM ports that appear when I connect J43 and J44 to my PC via USB ports.
I am writing a driver for a new sensor, and would like to view the printf statements being generated by the ISS server running on mcu2_0 to assist with debugging my code. Is there something special I need to do to enable this output?
Thanks.