This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62X: MCAN: Total bit rate tolerance [%]

Part Number: PROCESSOR-SDK-AM62X

Dear TI supporter,

I have run example mcan from mcu_plus_sdk_am62x_08_05_00_14 for CAN0.

This example is running with:

  • MCU_MCAN0_CLKSEL_CLK_SEL is utilized MCU_PLL0_HSDIV4_CLKOUT
  • The input clock frequency of MCU_MCAN0 that get in MCU_PLL0 is 80MHz

Currently I need to measure "Total bit rate tolerance" value

I think this parameter is provided by TI, so can you give me this parameter or if not is there a way to do or calculate this parameter with.

Best regards,

Hieu