Hello team,
Our customer is developing the next generation system with AM3354 (PROCESSOR-SDK-LINUX-AM335X, Version: 08.02.00.24, Kernel v5.10). According to "Getting Start Guide", it seems TI recommends customer to use gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf.tar.xz . but, instead of it, customer is asking if they are able to use " gcc 12.2" or not. Can I have your expert's advice/comments on this, please?
Best regards,
Miyazaki