This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6657: NDK can't sendto 10240 bytes

Genius 13655 points
Part Number: TMS320C6657


Hello Champs,

BIOS_MCSDK_2_1_2_6

NDK_2_23_02_03

pdk_C6678_1_1_2_6

Bios_6_33_06_50

xdias_7_21_01_07

xdctools_3_23_04_60

Compiler c6000_7.4.4

Customer modified NDK  to sendto 10240 bytes according to Enabling Jumbo Packet Support for C6678” and “Rebuilding The NDK Core Using Gmake - Texas Instruments Wiki". He can't catch any packet via wireshark. But the 1024 bytes can work. 

Code is stuck in continue,can't reach Line 771。


Customer also modified code according to below post.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/107053/pbm_alloc-for-transmit-packets



The issue still exists. 

Besides, after adding _INCLUDE_JUMBOFRAME_SUPPORT, it can't 1024bytes which works before. 


Thanks
Regards
Shine