Part Number: TDA4VM
Hello Team,
In the TDA4VM Technical Reference Manual (DRA829/TDA4VM Technical Reference Manual (Rev. C)), I found the following information with regards to CPSW 9-port switch ALE Automotive Security Features:
• VLANs can be configured to not allow fragmented IPv4 frames. That is a VLAN can be configured to not allow fragmented IPv4 traffic.
• VLANs can be configured to only allow up to four different IPv4 Protocols or IPv6. Next Header values, for example a VLAN can be configured to only allow TCP traffic in both IPv4 and IPv6 packets.
• Drop invalid Source Addresses, that is drop Source Addresses with bit 40 set (Multicast/Broadcast indicator on Destination Addresses)
• IEEE802.3 Length Check, drop frames that the IEEE802.3 Length is not contained within the frame. (Ether Types 0-1500)
• Any Source Address can be secured to a port dropping any attempts from other ports to masquerade as a service.
• Any source or destination address can be blocked.
• Per Port or Per VLAN ingress checking, dropping traffic from non-member ports.
• Classification, Policing on L2 and L3 information
However, I could not find any information regarding how to configure/enable these features. Could you please provide more information on how these features can be enabled in the CPSW switch?