Part Number: AM6442
Hi,
The customer tried to disable HS400 mode. Please see above original question.
He tried below configurations.
k3-am642-r5-evm.dts configuration:
&sdhci0 {
/delete-property/ power-domains;
clocks = <&clk_200mhz>;
clock-names = "clk_xin";
ti,driver-strength-ohm = <50>;
disable-wp;
pinctrl-0 = <&main_mmc0_pins_default>;
sdhci-caps-mask = <0x80000000 0x00000000>; /* disable HS400 speed mode */
};
k3-am642-evm.dts configuration:
&sdhci0 {
/* emmc */
bus-width = <8>;
non-removable;
ti,driver-strength-ohm = <50>;
disable-wp;
sdhci-caps-mask = <0x80000000 0x00000000>; /* disable HS400 speed mode */
};
But, it seems u-boot recognized eMMC card as HS400 mode.
=> mmcinfo
Device: mmc@fa10000
Manufacturer ID: 13
OEM: 14e
Name: S0J56
Bus Speed: 200000000
Mode: HS400 (200MHz)
Rd Block Len: 512
MMC version 5.1
Console log output:
U-Boot SPL 2021.01-dirty (Mar 23 2023 - 16:58:02 +0900) Resetting on cold boot to workaround ErrataID:i2331 resetting ... U-Boot SPL 2021.01-dirty (Mar 23 2023 - 16:58:02 +0900) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.7--v08.04.07 (Jolly Jellyfi') SPL initial stack usage: 13424 bytes Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Starting ATF on ARM64 core... NOTICE: BL31: v2.7(release):08.04.01.005 NOTICE: BL31: Built : 16:58:14, Mar 23 2023 U-Boot SPL 2021.01-dirty (Mar 23 2023 - 16:58:20 +0900) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.4.7--v08.04.07 (Jolly Jellyfi') Trying to boot from MMC2 Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted U-Boot 2021.01-dirty (Mar 23 2023 - 16:58:20 +0900) SoC: AM64X SR1.0 GP Model: Texas Instruments AM642 EVM Board: AM64-GPEVM rev E2 DRAM: 2 GiB NAND: 0 MiB MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from FAT... *** Warning - bad CRC, using default environment In: serial@2800000 Out: serial@2800000 Err: serial@2800000 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 => => mmcinfo Device: mmc@fa10000 Manufacturer ID: 13 OEM: 14e Name: S0J56 Bus Speed: 200000000 Mode: HS400 (200MHz) Rd Block Len: 512 MMC version 5.1 High Capacity: Yes Capacity: 14.8 GiB Bus Width: 8-bit DDR Erase Group Size: 512 KiB HC WP Group Size: 8 MiB User Capacity: 14.8 GiB WRREL Boot Capacity: 31.5 MiB ENH RPMB Capacity: 4 MiB ENH Boot area 0 is not write protected Boot area 1 is not write protected =>
Anything is wrong or missing?
Thanks and regards,
Koichiro Tashiro