This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Error of runing single cam on TDA4 with SDK0805

Part Number: TDA4VM

Hi TI experts,

I am doing camera IQ Tuning on TDA4VM with DCC2.5 based on the SDK version 0805.

I encountered errors showed below when I run "vx_app_single_cam.out", is this related to the parameters of H3A XMLs?

The whole logs is attached here:

5314.logs.txt
Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
root@optimus:/data# ./run_app_single_cam.sh
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
299.171262 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
299.171392 s: VX_ZONE_INIT:Enabled
299.171402 s: VX_ZONE_ERROR:Enabled
299.171410 s: VX_ZONE_WARNING:Enabled
299.173005 s: VX_ZONE_INIT:[tivxInitLocal:145] Initialization Done !!!
299.173287 s: VX_ZONE_INIT:[tivxHostInitLocal:93] Initialization Done for HOST !!!
sensor_selection = [0]
ldc_enable = [0]
num_frames_to_run = [1000000000]
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

and the H3A xmls are attached here too:

H3A_XML.zip

please help me check this error and H3A xml files, thanks.

  • Hi Zhili,

    That looks like the known bug in tuning tool V2.5 for wrong hskip and vskip encoding (they must be even numbers).

    Please upgrade to V3.0 available in mysecuresw a week ago.