This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash Tool - UART1 / URART3 - Unknown status message '?????????' during peripheral boot (waiting for 2nd)

I am using a custom Board with discrete Micron NAND-Flash 128MByte=1GB. So what I did is changed this line in omapflash2nd.txt

"CUSTOM_OMAP35XX_BOARD 343007 57 GP Targets\2nd-Downloaders\dnld_startup_omap3_gp_1g.2nd -pheriphalboot_reopen -board_config Targets\Configurations\configuration_custom_omap35xx.txt"

I set to NAND, SWECC, Erase region c0000 20000 (as this is the bootenvironment for test)

This ends up with:

¯ -stdout

¯ -omap 3

¯ -no_force_package_alignment

¯ -com 4

¯ -t 60

¯ -p CUSTOM_OMAP35XX_BOARD

¯ -2

¯ chip_erase NANDINFO1BITBOOT 00020000

¯ Leaving parameter file:temp_script.txt

¯ @temp_script.txt

¯ Looking for device (omap com4)

¯ Please turn off device, then turn it on again

¯ Awaiting ASIC id

¯ AsicId items 04

¯ AsicId id 01 05 01 34 30 07 57

¯ AsicId secure_mode 13 02 01 00

¯ AsicId public_id 12 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

¯ AsicId root_key_hash 14 15 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00

¯ Searching 2nd for: CUSTOM_OMAP35XX_BOARD 343007 57 GP

¯ Loading second file Targets\2nd-Downloaders\dnld_startup_omap3_gp_1g.2nd

¯ Entering parameter file:omapflash2nd.txt at line: 7

¯ -pheriphalboot_reopen

¯ Reading board configuration file Targets\Configurations\configuration_custom_omap35xx.txt

¯ Reading definition file .\targets\definitions\definitions_omap3.txt

¯ -board_config Targets\Configurations\configuration_custom_omap35xx.txt

¯ Leaving parameter file:omapflash2nd.txt

¯ Sending size of second file (0x00006804 bytes)

¯ Transferring second file to target (0x6804 bytes)

¯ Closing boot connection

¯ Found device (omap com4)

¯ Waiting for 2nd

¯ Unknown status message '?????????' during peripheral boot (waiting for 2nd)

Console program failed, exit code: 2

Question: Do I use the right 2nd - file ?

Currently my system is running on XLOADER that is very simular to EVM board, with the only difference, that UART3 keeps the interface for x-loader and uboot message