Part Number: TDA4VM
Hello,
The controller equipped with TDA4VM reports an error in the status of the eth_mac2_status during experiments in a high temperature environment.
And our operation is to obtain the Mac2_crc_Data and Mac2_carrier_Data of TDA4VM send it out through CAN, and when the data detected by the host computer is not 0, it is in an error state.
The register addresses are respectively (0x0C03A200UL+((2-1)*0x200) + 0x10UL) , (0x0C03A200UL+((2-1)*0x200) + 0x60UL).
We would like to see a description of these two values through the TI manual, and based on the first address we think it should be the register below.
However, the description is the storage of counter, and the state of the above two signals is not described.
So our doubts are:
1. Under what circumstances these two signals register returns a non-zero value?
2. Regarding the detection of eth_mac2_status, are we looking for the correct register address?

Thanks!