Other Parts Discussed in Thread: J7200XSOMXEVM, DRA821
Hello,
I have two questions.
TI's evaluation board (J7200XSOMXEVM) uses VDD_MCUIO_3V3 to power the PwrGrp: VDDSHV0_MCU.
1.If 3.3V from another system is used for the GPIO[INPUT] of PwrGrp:VDDSHV0_MCU, is there a possibility that 3.3V from another system will flow into VDDSHV0_MCU (E13/E14/F13/F14)?
"It means to use a separate 3.3V for the signal line like “①” in Fig. 1."
2.Also, is it possible with the DRA821 that the VDDSHV0_MCU voltage is also applied(wrap around) to another power group (eg VDDSHV2_MCU, etc.)?

best regards,