Hi,
According to the checklist:
EMIF
- Check that chip selects go to the proper memory for a correct memory map.
- For booting from NAND devices, make sure EMA_CS[3] is used.
- For booting from NOR devices, make sure EMA_CS[2] is used.
- Weak pullups are recommended on chip selects.
Should we add pullup resistors on the EMA_D0 ~ D7 also?
We will boot from Nand device.
Thanks
Jack