I don't see any requirements related to the clock speed of the packet accelerator subsystem. For example, what's the max input clock speed to this subsystem? (Please be clear on whether you are giving the clock speed before or after the hard-wired /2 coming out of the PASS PLL.) I expected to see requirements for the PLL itself too, i.e. min/max input clock frequency, min/max PLLOUT, etc.