This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts
When the system boot from eMMC, the reboot command cannot finally start the system, and the reset cannot be performed under uboot (the same problem exists on SK-AM62). But the reboot command works if booting from SD card. Can you please confirm how the reboot command should be used on eMMC boot?
Hi Bin
The rootfs in eMMC uses the tisdk-default-image-am62xx-evm.tar.xz in the filesystem in the SDK8.6. The bitbake compiled by customer only has the wic file, and there is no packaged tar.xz. This part still needs to be consulted. how do we get tar.xz file out?
By default the eMMC hardware reset signal RST_n is not enabled. Whether or not it should be permanently disabled or enabled can be configured one-time-only from within U-Boot:
In Uboot: mmc rst-function 0 1
OR:
In Linux: mmc hwreset enable /dev/mmcblk0