I decode 6 D1 h264 bit stream, and total bit rate is about 10Mbps.
But I use the 6 decoders at the same time, the output frames are something wrong.
The frame's x is 0 and y is very large number (like 3990752).
I use the 5 decoders at the same time, and they work fine.
Thanks & B/R,
Saige