This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interrupt Selector discrepancy between SPRU973 (TCP2 Ref Guide) and soc.h

The following snippet is from soc.h:

/* L2 Wakeup interrupt 0      */
#define    CSL_INTC_EVENTID_L2PDWAKE0       (30)       
/* L2 Wakeup interrupt 1      */
#define    CSL_INTC_EVENTID_L2PDWAKE1       (31)       
/* VCP2 error interrupt     */
#define    CSL_INTC_EVENTID_VCP2_INT        (32)       
/* TCP2 error interrupt     */
#define    CSL_INTC_EVENTID_TCP2_INT        (33)

The TCP2 documentation (SPRU973 pg 115, section 13.1) explicitly states that the interrupt selector for TCP2 errors is 31. The datasheet explicitly states that 30 & 31 are not valid events (unconnected) but agrees with soc.h about 32 & 33.

Is anyone able to confirm or correct the values in the above snippet for me? I am especially interested in the correct value for the TCP2 error interrupt.

Thank you,

Joseph Gagnon

Dyaptive Systems Inc.