This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding CE3CFG configuration in CCS

Other Parts Discussed in Thread: OMAP-L138

Hi,

Processor: OMAP-L138

I am running the NAND CCS project from CCS. I see that no where the code configures CE3CFG. Is it working because all the values are set to high?

I am loading the project from following path evmomapl138_v1\tests\evm\nand

Thank You & Regards,

GSR

  • GSR,

        If the code doesn't not configure a particular register, it should be at it's default value following a Power On Reset (Assuming there was not GEL file that modified the same register) before the code was run.