Hello,
I have two Davinci ARM devel board behaving the same way.
I received the latest devel board yesterday and it has all defaults, SD-card 2.6.37 512864-0001A.
I have two new Network PCIe 1x card based on RTL8168B, one behaves badly even on PC Linux, but the other is detected by lspci on PC Linux.
When I plug that "behaving" network card on the ARM PCIe slot, it stops Linux booting - last lines:
Running bootscript from MMC/SD to set the ENV...
## Executing script at 80900000
reading uImage
2362144 bytes read
## Booting kernel from Legacy Image at 80009000 ...
Image Name: Arago/2.6.37-psp04.00.00.10/dm81
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2362080 Bytes = 2.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
If PCIe RST is ON, then Linux boots but I never achieve to get anything in "ls /sys/bus/pci/devices", even after "echo 1 > /sys/bus/pci/rescan".
My aim is to be sure PCIe work, my company is planning to use Altera PCIe EP on this ARM PCIe RC on one single PCIe lane.
Any idea on what can be the problem?
Regards,
Etienne.