Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: AM6422
Hi,
We used AM6422 SR2 HS-FS on our customized board.
Do I have to re-build bl31.bin and bl32.bin, and then generate signed bl31.bin and bl32.bin? If so, what's the cmd to re-build them?
Or should I just use the pre-build GP bl31.bin and bl32.bin to generate the signed bl31.bin.signed and bl32.bin.signed?
When build the u-boot-spl.bin for tiboot3.bin and tispl.bin, u-boot.img, do I have to use the am64x_hs_evm_r5_defconfig and am64_hs_evm_a53_defconfig?

This picture shows that should use hs defconfig, but the following cmds show not use the hs defconfig.

These make me confused.
Best Regards
Xixiguohx