I loaded the images from http://www.jorjin.com.tw/TI_OMAP3530.html and the state on there web page "Note.To turn on WIFI function need firmware files, the©firmware.bin iscopy from TIPre-built Images."
Where do i put the the@firmware.bin file?
There are not any instructions nor does wi-fi work, i get an error when i try to turn on wi-fi.
I'm sure i have to put the .bin file some ware along with the wl1271 ini file but where?
Thanks
Bob