Hello,
The forum doesn't allow me to attach my tarball with sources, so please get it here: http://the-grue.de/~markus/myMsqQ.tar.bz2
After getting rid of code composer studio and instead using xdc / gmake on linux and Lee Holevas help (thanks!), I managed to "extract" syslinks "messageQ" example and compile it on its own. I want to modifiy it to create a simple telegram communication. I got along quite well, but now I'm stuck:
First, I got "region is invalid" assertion errors when calling HeapMemMP_open on Integras DSP (DSP/pt/msgq/MessageQApp.c::187)
/* Open the heap created by the other processor. Loop until opened. */
do {
status = HeapMemMP_open(aInfo.heapName, &heapHandle);
if (status == HeapMemMP_E_NOTFOUND) {
/* Sleep for a while before trying again. */
Task_sleep (10);
}
}
The assertain that failed was this one in line 203 of ipc_1_22_05_27/packages/ti/sdo/ipc/SharedRegion.c:
/* Make sure the region is valid */
Assert_isTrue(region->entry.isValid == TRUE,
ti_sdo_ipc_SharedRegion_A_regionInvalid);
Strangely enough, after some debugging with CCS, I don't get this assertin any more, but only because it seems that the APPNotify_callbackFxn is never called. When I start the test, nothing happens for a long time. When I stop the debugger I get this backtrace:

The breakpoint after the semaphore (DSP/pt/msgq/MessageQApp.c::180) is never reached.
It would be very kind if someone could have a look at it...
The versions of the used packages are:
ipc_1_22_05_27
syslink_02_00_00_68_beta1
TIA,
Markus