This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM64B: Problem with bitbake

Part Number: SK-AM64B

Hello,

I have recently purchased the SK-AM64B kit and I am having problems when building the SDK.  As my computer (Intel i7-1255U and 16GB Ram) runs Windows, I am using WSL2 and Ubuntu 18.04.5 LTS (instead of Virtual Box or VMWare).

It takes too much time to run this command:

MACHINE=am64xx-evm bitbake -k tisdk-default-image

Only 30% of the tasks have been completed after 24h.

NOTE: Executing Tasks
Currently 11 running tasks (2946 of 9383) 31% |###################### |
0: linux-ti-staging-5.10.168+gitAUTOINC+2c23e6c538-r0b.arago5 do_compile_kernelmodules - 4m57s (pid 1517)
1: binutils-2.34-r0 do_compile - 4m44s (pid 6607)
2: mariadb-native-10.4.25-r0 do_compile (pid 6806) 33% |#################### |
3: tcl-8.6.10-r0 do_install - 4m31s (pid 9159)
4: open62541-1.0.1+gitAUTOINC+e4309754fc-r0 do_compile (pid 9196) 0% | |
5: libmpc-1.1.0-r0 do_configure - 4m29s (pid 9282)
6: lame-3.100-r0 do_configure - 4m29s (pid 9296)
7: u-boot-ti-staging-1_2021.01+gitAUTOINC+2ee8efd654-r33 do_package - 4m28s (pid 9226)
8: faad2-2.8.8-r0 do_configure - 4m28s (pid 9317)
9: speex-1.2.0-r0 do_configure - 4m28s (pid 9307)
10: pulseaudio-13.0-r0 do_package - 4m20s (pid 10366)