This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: Configure AUDIO_EXT_REFCLK1

Expert 6650 points
Part Number: AM625

What is the correct way to enable a clock output on AUDIO_EXT_REFCLK1 pin?

 

We do have GPMC0_WPn (K25) pin that we would like to have it enabled and output a clock. From some old discussions it should be possible to have a 25MHz clock there.

  • Hi Isee,

    I am talking internally with the team on enabling clock on AUDIO_EXT_REFCLK1. Will get back to you as soon as I have an update.

    In the meantime, can you please share the k3conf dump clocks | grep AUDIO_EXT_REFLCK1  from the EVM with your DT changes in place.

    Thanks

    Suren

  • I found out that if I manually set the AUDIO_REFCLK1 to be output rather than the default input via CTRL_AUDIO_REFCLK1_CTRL register (Offset = 82E4h resp. 0x1082E4) bit 15 AUDIO_REFCLK1_CTRL_CLKOUT_EN (see section 6.1.1.3.1.160.1 CTRL_AUDIO_REFCLK1_CTRL Register on page 2688 of the latest TRM called SPRUIV7, https://www.ti.com/lit/pdf/SPRUIV7) it actually starts working. I did that via a utility called devmem2 which allows us to set arbitrary values at arbitrary memory/register addresses as follows:

    root@verdin-am62-14917624:~# devmem2 0x001082E4 w 0x00008007
    2/dev/mem opened.
    3Memory mapped at address 0xffff900f5000.
    4Read at address  0x001082E4 (0xffff900f52e4): 0x00000007
    5Write at address 0x001082E4 (0xffff900f52e4): 0x00008007, readback 0x00008007

    However, as the entire clock handling is done in TI’s proprietary system controller accessed from the Linux kernel only via TI SCI protocol, we have to assume this is actually a bug in that exact system controller implementation.

    BTW: Here is the link to the documented clocks ( https://software-dl.ti.com/tisci/esd/latest/5_soc_doc/am62x/clocks.html ) and as @Francesco Dolcini pointed out above we are indeed using device AM62X_DEV_BOARD0 with an ID of 157 and the DEV_BOARD0_AUDIO_EXT_REFCLK1_IN with a clock ID of 10 which should indeed be the clock we are looking for. Maybe the input vs. output nomenclature was too confusing even for TI’s own engineers Smirk.

    Can you please confirm this or suggest how exactly this is supposed to work? Thanks!

    We are working on the dumbs that you asked for.

  • Please find attached two full k3conf dump clocks one with 24.576 MHz (outputting 24.3901 MHz as verified by our HW folks) and the other one with 25 MHz. They were taken on our own Hardware (we do have the k3conf integrated into our BSP as well). 

    |--------------------------------------------------------------------------------|
    | VERSION INFO                                                                   |
    |--------------------------------------------------------------------------------|
    | K3CONF | (version v0.1-64-g48cb8e8 built Tue 04 Apr 2023 06:45:36 PM UTC)      |
    | SoC    | AM62X SR1.0                                                           |
    | SYSFW  | ABI: 3.1 (firmware version 0x0008 '8.5.3--v08.05.03 (Chill Capybar)') |
    |--------------------------------------------------------------------------------|
    
    autoadjust_table_generic_fprint(): WARNING: "DEV_BOARD0_OBSCLK0_IN_PARENT_SAM62_A53_512KB_WRAP_MAIN_0_ARM_COREPACK_0_A53_DIVH_CLK4_OBSCLK_OUT_CLKCLK_STATE_READY" size (115) > TABLE_MAX_ELT_LEN (100)!
    |---------------------------------------------------------------------------------------------------------------------------------------------------------------------|
    | Device ID | Clock ID | Clock Name                                                                                           | Status              | Clock Frequency |
    |---------------------------------------------------------------------------------------------------------------------------------------------------------------------|
    |   157     |     0    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN                                                                      | CLK_STATE_READY     | 24390243        |
    |   157     |     1    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     2    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     3    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     4    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     5    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     6    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     7    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_POSTDIV1_16FFT_MAIN_1_HSDIVOUT6_CLK                           | CLK_STATE_READY     | 96000000        |
    |   157     |     8    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT8_CLK                            | CLK_STATE_READY     | 24390243        |
    |   157     |     9    | DEV_BOARD0_AUDIO_EXT_REFCLK0_OUT                                                                     | CLK_STATE_READY     | 0               |
    |   157     |    10    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN                                                                      | CLK_STATE_READY     | 24390243        |
    |   157     |    11    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    12    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    13    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    14    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    15    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    16    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    17    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_POSTDIV1_16FFT_MAIN_1_HSDIVOUT6_CLK                           | CLK_STATE_READY     | 96000000        |
    |   157     |    18    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT8_CLK                            | CLK_STATE_READY     | 24390243        |
    |   157     |    19    | DEV_BOARD0_AUDIO_EXT_REFCLK1_OUT                                                                     | CLK_STATE_READY     | 0               |
    |   157     |    20    | DEV_BOARD0_CLKOUT0_IN                                                                                | CLK_STATE_READY     | 25000000        |
    |   157     |    21    | DEV_BOARD0_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT1_CLK5                                      | CLK_STATE_READY     | 50000000        |
    |   157     |    22    | DEV_BOARD0_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT1_CLK10                                     | CLK_STATE_READY     | 25000000        |
    |   157     |    23    | DEV_BOARD0_CP_GEMAC_CPTS0_RFT_CLK_OUT                                                                | CLK_STATE_READY     | 0               |
    |   157     |    24    | DEV_BOARD0_DDR0_CK0_IN                                                                               | CLK_STATE_READY     | 250000000       |
    |   157     |    25    | DEV_BOARD0_DDR0_CK0_N_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    27    | DEV_BOARD0_DDR0_CK0_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    33    | DEV_BOARD0_EXT_REFCLK1_OUT                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    34    | DEV_BOARD0_GPMC0_CLKLB_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    35    | DEV_BOARD0_GPMC0_CLKLB_OUT                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    36    | DEV_BOARD0_GPMC0_CLK_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    37    | DEV_BOARD0_GPMC0_FCLK_MUX_IN                                                                         | CLK_STATE_READY     | 133333333       |
    |   157     |    38    | DEV_BOARD0_GPMC0_FCLK_MUX_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT3_CLK                                | CLK_STATE_READY     | 133333333       |
    |   157     |    39    | DEV_BOARD0_GPMC0_FCLK_MUX_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT7_CLK                               | CLK_STATE_READY     | 100000000       |
    |   157     |    40    | DEV_BOARD0_I2C0_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    41    | DEV_BOARD0_I2C0_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    42    | DEV_BOARD0_I2C1_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    43    | DEV_BOARD0_I2C1_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    44    | DEV_BOARD0_I2C2_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    45    | DEV_BOARD0_I2C2_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    46    | DEV_BOARD0_I2C3_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    47    | DEV_BOARD0_I2C3_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    49    | DEV_BOARD0_MCASP0_ACLKR_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    50    | DEV_BOARD0_MCASP0_ACLKR_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    51    | DEV_BOARD0_MCASP0_ACLKX_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    52    | DEV_BOARD0_MCASP0_ACLKX_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    53    | DEV_BOARD0_MCASP0_AFSR_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    54    | DEV_BOARD0_MCASP0_AFSX_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    55    | DEV_BOARD0_MCASP1_ACLKR_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    56    | DEV_BOARD0_MCASP1_ACLKR_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    57    | DEV_BOARD0_MCASP1_ACLKX_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    58    | DEV_BOARD0_MCASP1_ACLKX_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    59    | DEV_BOARD0_MCASP1_AFSR_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    60    | DEV_BOARD0_MCASP1_AFSX_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    61    | DEV_BOARD0_MCASP2_ACLKR_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    62    | DEV_BOARD0_MCASP2_ACLKR_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    63    | DEV_BOARD0_MCASP2_ACLKX_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    64    | DEV_BOARD0_MCASP2_ACLKX_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    65    | DEV_BOARD0_MCASP2_AFSR_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    66    | DEV_BOARD0_MCASP2_AFSX_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    67    | DEV_BOARD0_MCU_EXT_REFCLK0_OUT                                                                       | CLK_STATE_READY     | 0               |
    |   157     |    68    | DEV_BOARD0_MCU_I2C0_SCL_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    69    | DEV_BOARD0_MCU_I2C0_SCL_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    70    | DEV_BOARD0_MCU_OBSCLK0_IN                                                                            | CLK_STATE_READY     | 12500000        |
    |   157     |    71    | DEV_BOARD0_MCU_OBSCLK0_IN_PARENT_MCU_OBSCLK_DIV_OUT0                                                 | CLK_STATE_READY     | 12500000        |
    |   157     |    72    | DEV_BOARD0_MCU_OBSCLK0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT                                             | CLK_STATE_READY     | 25000000        |
    |   157     |    73    | DEV_BOARD0_MCU_SPI0_CLK_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    75    | DEV_BOARD0_MCU_SPI1_CLK_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    77    | DEV_BOARD0_MCU_SYSCLKOUT0_IN                                                                         | CLK_STATE_READY     | 100000000       |
    |   157     |    78    | DEV_BOARD0_MCU_TIMER_IO0_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    79    | DEV_BOARD0_MCU_TIMER_IO1_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    80    | DEV_BOARD0_MCU_TIMER_IO2_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    81    | DEV_BOARD0_MCU_TIMER_IO3_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    82    | DEV_BOARD0_MDIO0_MDC_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    83    | DEV_BOARD0_MMC0_CLKLB_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    84    | DEV_BOARD0_MMC0_CLKLB_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    86    | DEV_BOARD0_MMC0_CLK_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    87    | DEV_BOARD0_MMC1_CLKLB_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    88    | DEV_BOARD0_MMC1_CLKLB_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    89    | DEV_BOARD0_MMC1_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    90    | DEV_BOARD0_MMC1_CLK_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    91    | DEV_BOARD0_MMC2_CLKLB_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    92    | DEV_BOARD0_MMC2_CLKLB_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    93    | DEV_BOARD0_MMC2_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    94    | DEV_BOARD0_MMC2_CLK_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    95    | DEV_BOARD0_OBSCLK0_IN                                                                                | CLK_STATE_READY     | 500000000       |
    |   157     |    96    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT0_CLK                                       | CLK_STATE_READY     | 500000000       |
    |   157     |    97    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_1_HSDIVOUT0_CLK                                       | CLK_STATE_READY     | 192000000       |
    |   157     |    98    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT0_CLK                                       | CLK_STATE_READY     | 333333333       |
    |   157     |    99    | DEV_BOARD0_OBSCLK0_IN_PARENT_SAM62_A53_512KB_WRAP_MAIN_0_ARM_COREPACK_0_A53_DIVH_CLK4_OBSCLK_OUT_CLK | CLK_STATE_READY     | 0               |
    |   157     |   100    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MAIN_12_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 400000000       |
    |   157     |   101    | DEV_BOARD0_OBSCLK0_IN_PARENT_GLUELOGIC_RCOSC_CLKOUT                                                  | CLK_STATE_READY     | 12500000        |
    |   157     |   102    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MCU_32KHZ_GEN_0_HSDIVOUT0_CLK8                             | CLK_STATE_READY     | 30637           |
    |   157     |   103    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT0_CLK_DUP0                                  | CLK_STATE_READY     | 500000000       |
    |   157     |   104    | DEV_BOARD0_OBSCLK0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT                                                 | CLK_STATE_READY     | 25000000        |
    |   157     |   105    | DEV_BOARD0_OBSCLK0_IN_PARENT_MAIN_OBSCLK0_MUX_SEL_DIV_CLKOUT                                         | CLK_STATE_READY     | 32552           |
    |   157     |   106    | DEV_BOARD0_OBSCLK0_IN_PARENT_CPSW_3GUSS_MAIN_0_CPTS_GENF0                                            | CLK_STATE_READY     | 0               |
    |   157     |   107    | DEV_BOARD0_OBSCLK0_IN_PARENT_CPSW_3GUSS_MAIN_0_CPTS_GENF1                                            | CLK_STATE_READY     | 0               |
    |   157     |   108    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MCU_0_HSDIVOUT0_CLK                                        | CLK_STATE_READY     | 400000000       |
    |   157     |   109    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV1_16FFT_MAIN_15_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 400000000       |
    |   157     |   110    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MAIN_16_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 1190000000      |
    |   157     |   111    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MAIN_17_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 170000000       |
    |   157     |   112    | DEV_BOARD0_OBSCLK0_IN_PARENT_SAM62_PLL_CTRL_WRAP_MAIN_0_CHIP_DIV1_CLK_CLK                            | CLK_STATE_READY     | 500000000       |
    |   157     |   113    | DEV_BOARD0_OBSCLK0_IN_PARENT_CLK_32K_RC_SEL_OUT0                                                     | CLK_STATE_READY     | 32768           |
    |   157     |   128    | DEV_BOARD0_OSPI0_DQS_OUT                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   129    | DEV_BOARD0_OSPI0_LBCLKO_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |   130    | DEV_BOARD0_OSPI0_LBCLKO_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |   131    | DEV_BOARD0_RGMII1_RXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   132    | DEV_BOARD0_RGMII1_TXC_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   133    | DEV_BOARD0_RGMII1_TXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   134    | DEV_BOARD0_RGMII2_RXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   135    | DEV_BOARD0_RGMII2_TXC_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   136    | DEV_BOARD0_RGMII2_TXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   137    | DEV_BOARD0_RMII1_REF_CLK_OUT                                                                         | CLK_STATE_READY     | 0               |
    |   157     |   138    | DEV_BOARD0_RMII2_REF_CLK_OUT                                                                         | CLK_STATE_READY     | 0               |
    |   157     |   139    | DEV_BOARD0_SPI0_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |   141    | DEV_BOARD0_SPI1_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |   143    | DEV_BOARD0_SPI2_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |   145    | DEV_BOARD0_SYSCLKOUT0_IN                                                                             | CLK_STATE_READY     | 125000000       |
    |   157     |   146    | DEV_BOARD0_TCK_OUT                                                                                   | CLK_STATE_READY     | 0               |
    |   157     |   147    | DEV_BOARD0_TIMER_IO0_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   148    | DEV_BOARD0_TIMER_IO1_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   149    | DEV_BOARD0_TIMER_IO2_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   150    | DEV_BOARD0_TIMER_IO3_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   151    | DEV_BOARD0_TIMER_IO4_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   152    | DEV_BOARD0_TIMER_IO5_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   153    | DEV_BOARD0_TIMER_IO6_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   154    | DEV_BOARD0_TIMER_IO7_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   155    | DEV_BOARD0_TRC_CLK_IN                                                                                | CLK_STATE_READY     | 0               |
    |   157     |   156    | DEV_BOARD0_VOUT0_EXTPCLKIN_OUT                                                                       | CLK_STATE_READY     | 0               |
    |   157     |   157    | DEV_BOARD0_VOUT0_PCLK_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   158    | DEV_BOARD0_WKUP_CLKOUT0_IN                                                                           | CLK_STATE_READY     | 25000000        |
    |   157     |   159    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT                                            | CLK_STATE_READY     | 25000000        |
    |   157     |   160    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_LFOSC0_CLKOUT                                            | CLK_STATE_READY     | 32768           |
    |   157     |   161    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT2_CLK                                  | CLK_STATE_READY     | 200000000       |
    |   157     |   162    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_1_HSDIVOUT2_CLK                                  | CLK_STATE_READY     | 192000000       |
    |   157     |   163    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT9_CLK                                 | CLK_STATE_READY     | 50000000        |
    |   157     |   164    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_CLK_32K_RC_SEL_OUT0                                                | CLK_STATE_READY     | 32768           |
    |   157     |   165    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_RCOSC_CLKOUT                                             | CLK_STATE_READY     | 12500000        |
    |   157     |   166    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT_DUP0                                       | CLK_STATE_READY     | 25000000        |
    |---------------------------------------------------------------------------------------------------------------------------------------------------------------------|
    
    

    |--------------------------------------------------------------------------------|
    | VERSION INFO                                                                   |
    |--------------------------------------------------------------------------------|
    | K3CONF | (version v0.1-64-g48cb8e8 built Tue 04 Apr 2023 06:45:36 PM UTC)      |
    | SoC    | AM62X SR1.0                                                           |
    | SYSFW  | ABI: 3.1 (firmware version 0x0008 '8.5.3--v08.05.03 (Chill Capybar)') |
    |--------------------------------------------------------------------------------|
    
    autoadjust_table_generic_fprint(): WARNING: "DEV_BOARD0_OBSCLK0_IN_PARENT_SAM62_A53_512KB_WRAP_MAIN_0_ARM_COREPACK_0_A53_DIVH_CLK4_OBSCLK_OUT_CLKCLK_STATE_READY" size (115) > TABLE_MAX_ELT_LEN (100)!
    |---------------------------------------------------------------------------------------------------------------------------------------------------------------------|
    | Device ID | Clock ID | Clock Name                                                                                           | Status              | Clock Frequency |
    |---------------------------------------------------------------------------------------------------------------------------------------------------------------------|
    |   157     |     0    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN                                                                      | CLK_STATE_READY     | 25000000        |
    |   157     |     1    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     2    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     3    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     4    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     5    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     6    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |     7    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_POSTDIV1_16FFT_MAIN_1_HSDIVOUT6_CLK                           | CLK_STATE_READY     | 96000000        |
    |   157     |     8    | DEV_BOARD0_AUDIO_EXT_REFCLK0_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT8_CLK                            | CLK_STATE_READY     | 25000000        |
    |   157     |     9    | DEV_BOARD0_AUDIO_EXT_REFCLK0_OUT                                                                     | CLK_STATE_READY     | 0               |
    |   157     |    10    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN                                                                      | CLK_STATE_READY     | 25000000        |
    |   157     |    11    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    12    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    13    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKR_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    14    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_0_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    15    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_1_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    16    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_MCASP_MAIN_2_MCASP_AHCLKX_POUT                                | CLK_STATE_NOT_READY | 0               |
    |   157     |    17    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_POSTDIV1_16FFT_MAIN_1_HSDIVOUT6_CLK                           | CLK_STATE_READY     | 96000000        |
    |   157     |    18    | DEV_BOARD0_AUDIO_EXT_REFCLK1_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT8_CLK                            | CLK_STATE_READY     | 25000000        |
    |   157     |    19    | DEV_BOARD0_AUDIO_EXT_REFCLK1_OUT                                                                     | CLK_STATE_READY     | 0               |
    |   157     |    20    | DEV_BOARD0_CLKOUT0_IN                                                                                | CLK_STATE_READY     | 25000000        |
    |   157     |    21    | DEV_BOARD0_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT1_CLK5                                      | CLK_STATE_READY     | 50000000        |
    |   157     |    22    | DEV_BOARD0_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT1_CLK10                                     | CLK_STATE_READY     | 25000000        |
    |   157     |    23    | DEV_BOARD0_CP_GEMAC_CPTS0_RFT_CLK_OUT                                                                | CLK_STATE_READY     | 0               |
    |   157     |    24    | DEV_BOARD0_DDR0_CK0_IN                                                                               | CLK_STATE_READY     | 250000000       |
    |   157     |    25    | DEV_BOARD0_DDR0_CK0_N_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    27    | DEV_BOARD0_DDR0_CK0_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    33    | DEV_BOARD0_EXT_REFCLK1_OUT                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    34    | DEV_BOARD0_GPMC0_CLKLB_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    35    | DEV_BOARD0_GPMC0_CLKLB_OUT                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    36    | DEV_BOARD0_GPMC0_CLK_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    37    | DEV_BOARD0_GPMC0_FCLK_MUX_IN                                                                         | CLK_STATE_READY     | 133333333       |
    |   157     |    38    | DEV_BOARD0_GPMC0_FCLK_MUX_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT3_CLK                                | CLK_STATE_READY     | 133333333       |
    |   157     |    39    | DEV_BOARD0_GPMC0_FCLK_MUX_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT7_CLK                               | CLK_STATE_READY     | 100000000       |
    |   157     |    40    | DEV_BOARD0_I2C0_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    41    | DEV_BOARD0_I2C0_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    42    | DEV_BOARD0_I2C1_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    43    | DEV_BOARD0_I2C1_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    44    | DEV_BOARD0_I2C2_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    45    | DEV_BOARD0_I2C2_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    46    | DEV_BOARD0_I2C3_SCL_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    47    | DEV_BOARD0_I2C3_SCL_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    49    | DEV_BOARD0_MCASP0_ACLKR_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    50    | DEV_BOARD0_MCASP0_ACLKR_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    51    | DEV_BOARD0_MCASP0_ACLKX_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    52    | DEV_BOARD0_MCASP0_ACLKX_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    53    | DEV_BOARD0_MCASP0_AFSR_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    54    | DEV_BOARD0_MCASP0_AFSX_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    55    | DEV_BOARD0_MCASP1_ACLKR_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    56    | DEV_BOARD0_MCASP1_ACLKR_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    57    | DEV_BOARD0_MCASP1_ACLKX_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    58    | DEV_BOARD0_MCASP1_ACLKX_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    59    | DEV_BOARD0_MCASP1_AFSR_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    60    | DEV_BOARD0_MCASP1_AFSX_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    61    | DEV_BOARD0_MCASP2_ACLKR_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    62    | DEV_BOARD0_MCASP2_ACLKR_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    63    | DEV_BOARD0_MCASP2_ACLKX_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    64    | DEV_BOARD0_MCASP2_ACLKX_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    65    | DEV_BOARD0_MCASP2_AFSR_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    66    | DEV_BOARD0_MCASP2_AFSX_IN                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    67    | DEV_BOARD0_MCU_EXT_REFCLK0_OUT                                                                       | CLK_STATE_READY     | 0               |
    |   157     |    68    | DEV_BOARD0_MCU_I2C0_SCL_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    69    | DEV_BOARD0_MCU_I2C0_SCL_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    70    | DEV_BOARD0_MCU_OBSCLK0_IN                                                                            | CLK_STATE_READY     | 12500000        |
    |   157     |    71    | DEV_BOARD0_MCU_OBSCLK0_IN_PARENT_MCU_OBSCLK_DIV_OUT0                                                 | CLK_STATE_READY     | 12500000        |
    |   157     |    72    | DEV_BOARD0_MCU_OBSCLK0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT                                             | CLK_STATE_READY     | 25000000        |
    |   157     |    73    | DEV_BOARD0_MCU_SPI0_CLK_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    75    | DEV_BOARD0_MCU_SPI1_CLK_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |    77    | DEV_BOARD0_MCU_SYSCLKOUT0_IN                                                                         | CLK_STATE_READY     | 100000000       |
    |   157     |    78    | DEV_BOARD0_MCU_TIMER_IO0_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    79    | DEV_BOARD0_MCU_TIMER_IO1_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    80    | DEV_BOARD0_MCU_TIMER_IO2_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    81    | DEV_BOARD0_MCU_TIMER_IO3_IN                                                                          | CLK_STATE_READY     | 0               |
    |   157     |    82    | DEV_BOARD0_MDIO0_MDC_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    83    | DEV_BOARD0_MMC0_CLKLB_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    84    | DEV_BOARD0_MMC0_CLKLB_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    86    | DEV_BOARD0_MMC0_CLK_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    87    | DEV_BOARD0_MMC1_CLKLB_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    88    | DEV_BOARD0_MMC1_CLKLB_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    89    | DEV_BOARD0_MMC1_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    90    | DEV_BOARD0_MMC1_CLK_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    91    | DEV_BOARD0_MMC2_CLKLB_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |    92    | DEV_BOARD0_MMC2_CLKLB_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |    93    | DEV_BOARD0_MMC2_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |    94    | DEV_BOARD0_MMC2_CLK_OUT                                                                              | CLK_STATE_READY     | 0               |
    |   157     |    95    | DEV_BOARD0_OBSCLK0_IN                                                                                | CLK_STATE_READY     | 500000000       |
    |   157     |    96    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT0_CLK                                       | CLK_STATE_READY     | 500000000       |
    |   157     |    97    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_1_HSDIVOUT0_CLK                                       | CLK_STATE_READY     | 192000000       |
    |   157     |    98    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT0_CLK                                       | CLK_STATE_READY     | 333333333       |
    |   157     |    99    | DEV_BOARD0_OBSCLK0_IN_PARENT_SAM62_A53_512KB_WRAP_MAIN_0_ARM_COREPACK_0_A53_DIVH_CLK4_OBSCLK_OUT_CLK | CLK_STATE_READY     | 0               |
    |   157     |   100    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MAIN_12_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 400000000       |
    |   157     |   101    | DEV_BOARD0_OBSCLK0_IN_PARENT_GLUELOGIC_RCOSC_CLKOUT                                                  | CLK_STATE_READY     | 12500000        |
    |   157     |   102    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MCU_32KHZ_GEN_0_HSDIVOUT0_CLK8                             | CLK_STATE_READY     | 30637           |
    |   157     |   103    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT0_CLK_DUP0                                  | CLK_STATE_READY     | 500000000       |
    |   157     |   104    | DEV_BOARD0_OBSCLK0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT                                                 | CLK_STATE_READY     | 25000000        |
    |   157     |   105    | DEV_BOARD0_OBSCLK0_IN_PARENT_MAIN_OBSCLK0_MUX_SEL_DIV_CLKOUT                                         | CLK_STATE_READY     | 32552           |
    |   157     |   106    | DEV_BOARD0_OBSCLK0_IN_PARENT_CPSW_3GUSS_MAIN_0_CPTS_GENF0                                            | CLK_STATE_READY     | 0               |
    |   157     |   107    | DEV_BOARD0_OBSCLK0_IN_PARENT_CPSW_3GUSS_MAIN_0_CPTS_GENF1                                            | CLK_STATE_READY     | 0               |
    |   157     |   108    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV4_16FFT_MCU_0_HSDIVOUT0_CLK                                        | CLK_STATE_READY     | 400000000       |
    |   157     |   109    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV1_16FFT_MAIN_15_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 400000000       |
    |   157     |   110    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MAIN_16_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 1190000000      |
    |   157     |   111    | DEV_BOARD0_OBSCLK0_IN_PARENT_HSDIV0_16FFT_MAIN_17_HSDIVOUT0_CLK                                      | CLK_STATE_READY     | 170000000       |
    |   157     |   112    | DEV_BOARD0_OBSCLK0_IN_PARENT_SAM62_PLL_CTRL_WRAP_MAIN_0_CHIP_DIV1_CLK_CLK                            | CLK_STATE_READY     | 500000000       |
    |   157     |   113    | DEV_BOARD0_OBSCLK0_IN_PARENT_CLK_32K_RC_SEL_OUT0                                                     | CLK_STATE_READY     | 32768           |
    |   157     |   128    | DEV_BOARD0_OSPI0_DQS_OUT                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   129    | DEV_BOARD0_OSPI0_LBCLKO_IN                                                                           | CLK_STATE_READY     | 0               |
    |   157     |   130    | DEV_BOARD0_OSPI0_LBCLKO_OUT                                                                          | CLK_STATE_READY     | 0               |
    |   157     |   131    | DEV_BOARD0_RGMII1_RXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   132    | DEV_BOARD0_RGMII1_TXC_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   133    | DEV_BOARD0_RGMII1_TXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   134    | DEV_BOARD0_RGMII2_RXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   135    | DEV_BOARD0_RGMII2_TXC_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   136    | DEV_BOARD0_RGMII2_TXC_OUT                                                                            | CLK_STATE_READY     | 0               |
    |   157     |   137    | DEV_BOARD0_RMII1_REF_CLK_OUT                                                                         | CLK_STATE_READY     | 0               |
    |   157     |   138    | DEV_BOARD0_RMII2_REF_CLK_OUT                                                                         | CLK_STATE_READY     | 0               |
    |   157     |   139    | DEV_BOARD0_SPI0_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |   141    | DEV_BOARD0_SPI1_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |   143    | DEV_BOARD0_SPI2_CLK_IN                                                                               | CLK_STATE_READY     | 0               |
    |   157     |   145    | DEV_BOARD0_SYSCLKOUT0_IN                                                                             | CLK_STATE_READY     | 125000000       |
    |   157     |   146    | DEV_BOARD0_TCK_OUT                                                                                   | CLK_STATE_READY     | 0               |
    |   157     |   147    | DEV_BOARD0_TIMER_IO0_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   148    | DEV_BOARD0_TIMER_IO1_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   149    | DEV_BOARD0_TIMER_IO2_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   150    | DEV_BOARD0_TIMER_IO3_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   151    | DEV_BOARD0_TIMER_IO4_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   152    | DEV_BOARD0_TIMER_IO5_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   153    | DEV_BOARD0_TIMER_IO6_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   154    | DEV_BOARD0_TIMER_IO7_IN                                                                              | CLK_STATE_READY     | 0               |
    |   157     |   155    | DEV_BOARD0_TRC_CLK_IN                                                                                | CLK_STATE_READY     | 0               |
    |   157     |   156    | DEV_BOARD0_VOUT0_EXTPCLKIN_OUT                                                                       | CLK_STATE_READY     | 0               |
    |   157     |   157    | DEV_BOARD0_VOUT0_PCLK_IN                                                                             | CLK_STATE_READY     | 0               |
    |   157     |   158    | DEV_BOARD0_WKUP_CLKOUT0_IN                                                                           | CLK_STATE_READY     | 25000000        |
    |   157     |   159    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT                                            | CLK_STATE_READY     | 25000000        |
    |   157     |   160    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_LFOSC0_CLKOUT                                            | CLK_STATE_READY     | 32768           |
    |   157     |   161    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_0_HSDIVOUT2_CLK                                  | CLK_STATE_READY     | 200000000       |
    |   157     |   162    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_HSDIV4_16FFT_MAIN_1_HSDIVOUT2_CLK                                  | CLK_STATE_READY     | 192000000       |
    |   157     |   163    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_POSTDIV4_16FF_MAIN_2_HSDIVOUT9_CLK                                 | CLK_STATE_READY     | 50000000        |
    |   157     |   164    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_CLK_32K_RC_SEL_OUT0                                                | CLK_STATE_READY     | 32768           |
    |   157     |   165    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_RCOSC_CLKOUT                                             | CLK_STATE_READY     | 12500000        |
    |   157     |   166    | DEV_BOARD0_WKUP_CLKOUT0_IN_PARENT_GLUELOGIC_HFOSC0_CLKOUT_DUP0                                       | CLK_STATE_READY     | 25000000        |
    |---------------------------------------------------------------------------------------------------------------------------------------------------------------------|
    
    

  • Hi Isee,

    Thanks for the details and dumps.

    Just wanted to update you that we are internally working on having this fixed in our software. This would be fixed in our next SDK release.

    Thanks,

    Suren