Other Parts Discussed in Thread: TMS320C6747
Hi, My processor clock is external 40MHz. Is there any problem to boot my processor in SPI Flash mode? Is there any specific frequency requirement for SPI boot? Anulal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320C6747
Hi, My processor clock is external 40MHz. Is there any problem to boot my processor in SPI Flash mode? Is there any specific frequency requirement for SPI boot? Anulal
Hi Anulal,
Refer to these documents.
1. TMS320C674x/OMAP-L1x Processor Serial Peripheral Interface (SPI) User's Guide
http://focus.ti.com/lit/ug/sprufm4i/sprufm4i.pdf
2. Using the TMS320C6747/45/43 Bootloader
Page 24; Boot Requirements, Constraints and Default Settings
http://focus.ti.com/lit/an/sprabb1b/sprabb1b.pdf
Hope this helps.
Best Regards,
Ankit Agrawal
HI ankit,
Thank you for your help.
I've went through sprabb1b.pdf (Bootloader application note). In Table 4. "Default Clock Configurations for Various Boot Modes" SPI clock frequency for 24MHz input and 25MHz is given. Does it mean that the input clock should be either 24/25 MHz? For other boot modes possible values of clocks are given.
Anulal
Anulal,
The default clock frequency was intended to be around 1 MHz for SPI memory devices. Most SPI flash or EEPROM can run much faster than this, but this lower frequency is intended to offer broad compatibility, and users can update the clock settings during the boot, via some AIS commands, to get the clock to run faster. When using an input clock of 40MHz, the default frequency will scale to be ~1.54 MHz (0.962 *40/25). That should be fine, but you should double check with your SPI memory datasheet to verify. If you scale the clock during the boot, make sure you scale using appropriate multipliers and dividers to account for using a 40 MHz input.
Regards, Daniel