Other Parts Discussed in Thread: AM1707
We port Davinci-PSP-SDK-03.20.00.12 on an AM1707 board.
Now linux can boot to show the shell, but have many "BUG: Bad page state in process xxx" report.
Can somebody give us some tip?
Thanks a lot!
...
[ 2.850000] VFS: Mounted root (nfs filesystem) on device 0:13.
[ 2.870000] devtmpfs: mounted
[ 2.880000] Freeing init memory: 84K
[ 3.470000] BUG: Bad page state in process hostname pfn:c06cc
[ 3.480000] page:c033e980 flags:0000000c count:0 mapcount:1 mapping:c05a6cb4 index:a5
[ 3.500000] [<c002232c>] (unwind_backtrace+0x0/0xd0) from [<c00671c4>] (bad_page+0x104/0x138)
[ 3.510000] [<c00671c4>] (bad_page+0x104/0x138) from [<c00777d8>] (unmap_vmas+0x3a0/0x638)
[ 3.510000] [<c00777d8>] (unmap_vmas+0x3a0/0x638) from [<c007a28c>] (exit_mmap+0xc4/0x204)
[ 3.520000] [<c007a28c>] (exit_mmap+0xc4/0x204) from [<c0031694>] (mmput+0x38/0xec)
[ 3.520000] [<c0031694>] (mmput+0x38/0xec) from [<c003549c>] (exit_mm+0x11c/0x124)
[ 3.530000] [<c003549c>] (exit_mm+0x11c/0x124) from [<c0036b30>] (do_exit+0x18c/0x658)
[ 3.530000] [<c0036b30>] (do_exit+0x18c/0x658) from [<c00370b4>] (do_group_exit+0xb8/0xec)
[ 3.540000] [<c00370b4>] (do_group_exit+0xb8/0xec) from [<c00370f8>] (sys_exit_group+0x10/0x1c)
[ 3.550000] [<c00370f8>] (sys_exit_group+0x10/0x1c) from [<c001dea0>] (ret_fast_syscall+0x0/0x28)
[ 3.550000] Disabling lock debugging due to kernel taint
System initialization...
Hostname : OMAP3EVM
Filesystem : v1.0.0
[ 3.780000] BUG: Bad page state in process uname pfn:c06cc
[ 3.790000] page:c033e980 flags:0000000c count:0 mapcount:1 mapping:c05a6cb4 index:a5
[ 3.810000] [<c002232c>] (unwind_backtrace+0x0/0xd0) from [<c00671c4>] (bad_page+0x104/0x138)
[ 3.820000] [<c00671c4>] (bad_page+0x104/0x138) from [<c00777d8>] (unmap_vmas+0x3a0/0x638)
[ 3.820000] [<c00777d8>] (unmap_vmas+0x3a0/0x638) from [<c007a28c>] (exit_mmap+0xc4/0x204)
[ 3.830000] [<c007a28c>] (exit_mmap+0xc4/0x204) from [<c0031694>] (mmput+0x38/0xec)
[ 3.830000] [<c0031694>] (mmput+0x38/0xec) from [<c003549c>] (exit_mm+0x11c/0x124)
[ 3.840000] [<c003549c>] (exit_mm+0x11c/0x124) from [<c0036b30>] (do_exit+0x18c/0x658)
[ 3.850000] [<c0036b30>] (do_exit+0x18c/0x658) from [<c00370b4>] (do_group_exit+0xb8/0xec)
[ 3.850000] [<c00370b4>] (do_group_exit+0xb8/0xec) from [<c00370f8>] (sys_exit_group+0x10/0x1c)
[ 3.860000] [<c00370f8>] (sys_exit_group+0x10/0x1c) from [<c001dea0>] (ret_fast_syscall+0x0/0x28)
[ 3.860000] BUG: Bad page state in process uname pfn:c06e0
[ 3.870000] page:c033ec00 flags:0000000c count:0 mapcount:1 mapping:c05a6cb4 index:c7
...
/ #