This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: OSPI Slave?

Part Number: AM623

Asking on behalf of customer:


we would like to use OSPI to transfer data between TI AM6234 (through DMA) with FPGA, we would like to understand if we can make FPGA as master instead of slave?

Should we create a flash like memory in FPGA to act like OSPI flash in slave mode in order to use OSPI?

Or FPGA can act as master and transfer data through OSPI?


It appears that in the QSPI.html doc in the Kernel drivers that OSPI and QSPI can only be used in master mode when used as a memory mapped IO interface.  Is there some other mode OSPI could be used here that would allow AM623 to be a slave?

Thanks!

-Steve