Other Parts Discussed in Thread: OMAP3530
Hi, I am a beginner in DSP and shared memory ... I tried to run the message application and it run correctly, then i edited the message sample to calculate the FFT on DSP core, when i ran the application on OMAP3530 this fault is shown to me: DSP MMU Error Fault! MMU_IRQSTATUS = [0x1]. Virtual DSP addr reference that generated the interrupt = [0x87dffff8]. then i tried to configure the the CFG_OMAP3530_SHMEM.c file to increase the size of the shared memory , and I get the same error, at the same time i configured the dsplink-omap3530-base.tci file and no result.... thanks Ahmed Abdullah