This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

av_server of DM368IPNC-IMX035_V2.00.22 by APPRO

Hi, My name is sungho Jang.

Please give me any advise. Thanks.

Av_server sometimes dies without any error messages even though it has been running well until the moment.

In the upper case, the codec configuration information is like below

- First stream : 1080P, FPS 3, GOP 3, Bit-Rate 12000kpbs, bit-rate-Control : CBR

- Second stream : QVGA, FPS 3, GOP 3, Bit-Rate 3000kpbs, bit-rate-Control : CBR

However, I have found that it never dies when FPS is 30 and GOP is 30.

Is there any problem with av_server of DM368IPNC-IMX035_V2.00.22 provided by APPRO when FPS is low and bitrate is high?