Part Number: PROCESSOR-SDK-AM62X
hello ti,
we are using custom board with am6254, I see below kernel panic in latest sdk v08.06, can you please help?
[ 8.450502] Internal error: synchronous external abort: 96000010 [#1] PREEMPT SMP [ 8.457996] Modules linked in: pruss(+) pvrsrvkm(O) sch_fq_codel cryptodev(O) ipv6 [ 8.465584] CPU: 1 PID: 380 Comm: systemd-udevd Tainted: G O 5.10.16848784d7cb #1 [ 8.474377] Hardware name: HARMAN Z067 DMS (DT) [ 8.478959] pstate: 20000005 (nzCv daif -PAN -UAO -TCO BTYPE=--) [ 8.478982] pc : clk_mux_get_parent+0x18/0x80 [ 8.478987] lr : __clk_init_parent+0x3c/0x58 [ 8.478990] sp : ffff800011c3b580 [ 8.478993] x29: ffff800011c3b580 x28: ffff0000058b76d0 [ 8.479002] x27: 0000000000000002 x26: 0000000000000001 [ 8.479007] x25: 0000000000000000 x24: ffff000003f18180 [ 8.479013] x23: ffff0000058b7680 x22: ffff000005778480 [ 8.479018] x21: ffff0000058b7400 x20: ffff0000058b7580 [ 8.479023] x19: ffff0000058c2700 x18: 0000000000000020 [ 8.479028] x17: 0000000000000000 x16: 0000000000000000 [ 8.479033] x15: ffffffffffffffff x14: ffffffffff000000 [ 8.479038] x13: ffffffffffffffff x12: 0000000000000008 [ 8.479043] x11: 0000000000000001 x10: 0101010101010101 [ 8.479048] x9 : 0000000000000000 x8 : 7f7f7f7f7f7f7f7f [ 8.479053] x7 : 6261735e6c766f64 x6 : 564047596f445253 [ 8.479058] x5 : 5352446f59474056 x4 : ffff800011b8903c [ 8.479063] x3 : 6660606860606060 x2 : ffff800010653a18 [ 8.479068] x1 : 0000000000000000 x0 : ffff0000058b7580 [ 8.479075] Call trace: [ 8.479083] clk_mux_get_parent+0x18/0x80 [ 8.479087] __clk_init_parent+0x3c/0x58 [ 8.479091] __clk_register+0x39c/0x7c0 [ 8.479096] clk_hw_register+0x20/0x60 [ 8.479101] __clk_hw_register_mux+0x140/0x1c8 [ 8.479105] clk_register_mux_table+0x4c/0x68 [ 8.479121] pruss_clk_mux_setup.isra.0+0x10c/0x238 [pruss] [ 8.479128] pruss_cfg_of_init+0x198/0x258 [pruss] [ 8.479135] pruss_probe+0x1a4/0x38c [pruss] [ 8.479143] platform_drv_probe+0x54/0xa8 [ 8.479148] really_probe+0xf0/0x500 [ 8.479152] driver_probe_device+0xf4/0x160 [ 8.479156] device_driver_attach+0x74/0x80 [ 8.479159] __driver_attach+0xc8/0x188 [ 8.479166] bus_for_each_dev+0x70/0xc0 [ 8.479170] driver_attach+0x24/0x30 [ 8.479174] bus_add_driver+0x148/0x238 [ 8.479178] driver_register+0x64/0x120 [ 8.479182] __platform_driver_register+0x48/0x58 [ 8.479189] pruss_driver_init+0x24/0x1000 [pruss] [ 8.479196] do_one_initcall+0x44/0x2d0 [ 8.479205] do_init_module+0x48/0x1f0 [ 8.479210] load_module+0x2300/0x29e8 [ 8.479214] __do_sys_finit_module+0xbc/0x128 [ 8.479218] __arm64_sys_finit_module+0x20/0x30 [ 8.479227] el0_svc_common.constprop.0+0x78/0x1c8 [ 8.479231] do_el0_svc+0x24/0xa0 [ 8.479242] el0_svc+0x14/0x20 [ 8.479246] el0_sync_handler+0xb0/0xb8 [ 8.479249] el0_sync+0x180/0x1c0 [ 8.479259] Code: 910003fd 3940b401 f9400c04 37280201 (b9400084) [ 8.479268] ---[ end trace 94fbc5d460f6de5a ]---