Hi,
Below are few queries on the AM389X. Kindly provide your inputs.
1) Is there any "PMIC" available for AM389X processor (to generate 3.3V, 1V_CON, 1V_AVS, 1.8V, 1.5V and 0.9V) ?
2) Where can i find the "maximum current consumptions" for the above mentioned power rails ?
3) Is there any "heatsink" requirement for this AM389X ?
4) What is the "default voltage" expected on 1V_AVS power rail during the "processor power up" ?
5) My understanding is that Smartreflex adopts AVS. so, how actually does "smartreflex inform the processor" for any voltage change requirement ? We need to implement the same in our design.
Thanks in advance for your replies.
Warm regards,
Prajwal Kini A.