Hi,
Board is custom board refer to AM574x IDK ,modified power unit and changed ddr3(AM5749, DDR3/L :IGB13H8G162BF-13KI 2pic ,ECC DDR3/L :IGB13H8G802BF-13KI 1pic)
U-boot version is "u-boot-2019.01+gitAUTOINC+333c3e72d3-g333c3e72d3"
DEVICE_TREE=am574x-idk
Config used am57xx_evm_defconfig
I used CCS V12.2.0 debugger run "step over" to trace this issue.
The code will into _main() --> memset then jump to 0x0000000c PRUSS1_CFG_PRUSS_GPCFG1 and stop at here.