Other Parts Discussed in Thread: AM3517
hi,
I am using AM3517 custom board.
Booting is from MMC1 and i am using uart3. the board will boot up and stops in bootloader but i am not able to give the input to the processor that means when i type any character in the serial console some junk characters will appear but when i probed and checked the UART3_RX signal will come for UART3_RX_IRRX (P1).
i am using teraterm-4.66 and baud rate is 115200 with one stop bit.
while booting the messing or comming properly that means processor is sending properly.
thanks,
srikanth H.V