Hi,
Could you tell us how we can change the peripheral value to 80 (QSPI) in the "Table 4-51. Boot Parameter Table Common Header" from DRA829V TRM ?
Regards,
Hideaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could you tell us how we can change the peripheral value to 80 (QSPI) in the "Table 4-51. Boot Parameter Table Common Header" from DRA829V TRM ?
Regards,
Hideaki
Hi Robert,
Thank you for your reply.
They set the BOOT pins as QSPI boot, and QSPI boot was successful. However, "Peripheral" of Boot Parameter Table Common Header indicates "85" OSPI, not "80" QSPI. Why is it ? How can they set it correctly ?
Thanks and regards,
Hideaki
Hi Matsumoto-san,
As Robert is out until Monday, I will try to fill in. Based on the DIP switch settings for OSPI found in the SDK documentation's Boot Modes(link) section and for QSPI a FAQ(link) from my colleague, this is how OSPI and QSPI are set:
Referencing the EVM(link) userguide's Table 3-8, setting SW9.3 high for QSPI and setting SW9.2 high for OSPI are both setting "Primary Boot Mode A". ROM code will read these pins to determine whether to boot from QSPI vs OSPI.
Does this answer your question?
Regards,
Takuma