Other Parts Discussed in Thread: TVP5146, OMAPL138
hello everyone,
I've just finished building a FileSystem+Kernel Image from arago, with kernel linux-davinci-2.6.37-psp03.21.00.04.sdk-r57.
everything seems to be working, aside from one problem: v4l2 isn't working
every time I try to run dmai/ce example / gstreamer pipeline / manually read from /dev/video0 I'm getting the following error:
invalid media connection to video node
invalid external subdev
My bootargs are:
console=ttyS0,115200n8 noinitrd rw ip=192.168.1.2 root=/dev/nfs nfsroot=192.168.1.1:/home/user/workdir365/rootfs,nolock mem=60M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=1 davinci_display.cont2_bufsize=6291456 vpfe_capture.bufsize=829440davinci_enc_mngr.ch0_mode=pal vpfe_capture.interface=0
dmesg after boot:
I've looked in the kernel sources and it looks like the failure occurs in vpfe_video.c, but I have no idea why any function there would fail since tvp5146 was registered OK
any help would be great!
Thanks,
James