This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSP Drivers enableCache setting in C674x



Hi,  I just wanted to confirm that when using the EDMA modes of peripherals with the PSP, that the enableCache configuration setting for most of the peripherals needs to be set to TRUE if the data buffers are in any of the RAMs not in the megamodule (eg SDRAM) .  If using a data block from L2 RAM (or L1, if configured that way for that matter), then hw should take care of cache coherency, and this can be set to FALSE for increased performance, correct?

Thanks!

Peter