This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: Transplant codesys runtime

Part Number: SK-AM62

Hi,

1. Can Codesys Runtime for ARM64 be installed directly through the install in the Codesys software, or can it only be transplanted? The transplant process is as follows:

https://dev.ti.com/tirex/explore/node?node=A__AEo80w6KenaXT3E67VNzxg__linux_academy_am62x__XaWts8R__LATEST

2. Refer to the above link to copy by scp, is it to copy the entire CODESYS Control for Linux ARM64 SL folder, or just two files? Is it possible to directly put codemeter-lite_7.21.4611.501_arm64.deb and codesyscontrol_linuxarm64_4.2.0.0_arm64.deb in the root directory of the SD card using the host computer?