This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: VSS_RTC connect to VSS

Guru 10136 points

Part Number: AM3354

Hi TI

A customer is inquiring about the difference between Datasheet and EVM Schematic for VSS_RTC processing.
Can I understand that VSS on Datasheet and GND_OSC1 on EVM circuit diagram are the same? Or ask if EVM designed it without following the guide. I think GND_OSC1 is the nearest PCB digital ground VSS...

TI, please explain. ^^

Thanks

Regards, 

Jack

  • Hello Jack, 

    Thank you for the query.

    Can I understand that VSS on Datasheet and GND_OSC1 on EVM circuit diagram are the same? Or ask if EVM designed it without following the guide. I think GND_OSC1 is the nearest PCB digital ground VSS...

    The grounds that you are referencing seems correct.  VSS_OSC and VSS_RTC are required to be connected to system ground.

    Please refer below section of the AM335x Schematic Checklist

    2.5 Clocking

    • If you do not need RTC-only mode and the RTC timer feature, you do not need to include a 32 KHz crystal. The 32 KHz reference can come from the high frequency clock. Leave the RTC_XTALIN/RTC_XTALOUT pins as NC.

    • Per Advisory 1.0.30 in the device Silicon Errata, VSS_OSC and VSS_RTC should be connected to system ground.

    • It is preferable to always have bias and dampening resistors that can help tune the crystal later. For more details, see the Clock Specifications section of the device-specific data sheet.

    Please refer below BBB schematics for implementation 

    Whenever there is a discrepancy between the Datasheet and EVM, it is recommended to follow the datasheet.

    Regards,

    Sreenivasa