This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About NAND boot

Genius 3400 points


Hi all,

     We modify our Camera board(no modify nand module). It cannot boot from NAND, just see in following:

DM36x initialization passed!
TI UBL Version: 1.50 2010-11-12
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000019.
DONE
Jumping to entry point at 0x81080000.  //It's pause at here.

and the new camera board can boot successfully from SD. 

The old camera board can boot from SD and nand successfully. 

Our hardware engineer said they had not modify the nand module.

Anybody can give me some advices? 


  • Did you remove the alarm pin in your board.  If the alarm in is not pull high the boot will go into a diagnostic mode.  You have to modify UBL.

  • Thank your reply!

    We had fond what's reason.

    If we come down the DDR frequency in Uboot setting. it can work correctly.

    We will find what's reason lead to the limit.

     

  • Hi all,    

          It's still boot  from nand problem that we modify our Camera board(using DM368). The old board, we set DDR PLL to 343, and can boot from nand successfully. But the new board cannot.

         we set different DDR PLL in uboot, the phenomena is different: Set the DDR PLL to 300M or below, it can boot successfully; Set the DDR PLL 320M or 343M, it can not boot, and the error message is different. just as see the following.

         Set DDR PLL to 240/300M in uboot, it can boot successfully:

    TI UBL Version: 1.50 2011-07-14 16:35
    Booting Catalog Boot Loader
    BootMode = NAND
    Starting NAND Copy...
    Valid magicnum, 0xA1ACED66, found in block 0x00000019.
       DONE
    Jumping to entry point at 0x81080000.

    Boot 2009.03-svn ( 5鏈?25 2011 - 17:48:45)  2011-05-25

    I2C:   ready
    DRAM: 256 MB
    NAND:  NAND device: Manufacturer ID: 0x2c, Chip ID: 0x48 (Micron NAND 2GiB 3,3V 8-bit)
    2048 MiB
    *** Warning - bad CRC or NAND, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Ethernet PHY: GENERIC @ 0x01
    Hit any key to stop autoboot:  0

    NAND read: device 0 offset 0x2400000, size 0x100
     256 bytes read: OK

    NAND read: device 0 offset 0xb400000, size 0xa00000
     10485760 bytes read: OK
    check cramfs crc ok 0x76100162

    Loading from NAND 2GiB 3,3V 8-bit, offset 0xb000000
       Image Name:   Linux-2.6.18_pro500-davinci_IPNC
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1839788 Bytes =  1.8 MB
       Load Address: 80008000
       Entry Point:  80008000
    ## Booting kernel from Legacy Image at 80700000 ...
       Image Name:   Linux-2.6.18_pro500-davinci_IPNC
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1839788 Bytes =  1.8 MB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux........................................................................................................................... done, booting the kernel.
    Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.0_20110706-test (zhangjp@localhost.localdomain) (gcc 鐗堟湰 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Wed May 18 16:25:45 CST 2011 2010-11-18
    CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
    Machine: DaVinci DM368 IPNC
    Memory policy: ECC disabled, Data cache writeback
    DaVinci DM0365 variant 0x8
    PLL0: fixedrate: 24000000, commonrate: 121500000, vpssrate: 243000000
    PLL0: vencrate_sd: 27000000, ddrrate: 243000000 mmcsdrate: 121500000
    PLL1: armrate: 297000000, voicerate: 20482758, vencrate_hd: 74250000
    CPU0: D VIVT write-back cache
    CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
    CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
    Built 1 zonelists.  Total pages: 24576
    Kernel command line: mem=96M console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x82000000,10M ip=192.168.0.231:192.168.0.2:192.168.0.2:255.255.255.0:::off eth=00:21:49:00:00:35
    TI DaVinci EMAC: kernel boot params Ethernet address: 00:21:49:00:00:35
    PID hash table entries: 512 (order: 9, 2048 bytes)
    Clock event device timer0_0 configured with caps set: 07
    Console: colour dummy device 80x30
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 96MB = 96MB total
    Memory: 83072KB available (3141K code, 651K data, 180K init)
    Security Framework v1.0.0 initialized
    Capability LSM initialized .......

    if we set DDR PLL to 320M and up in uboot, it cannot boot from nand:

    DM36x initialization passed!
    TI UBL Version: 1.50 2011-07-14 16:35
    Booting Catalog Boot Loader
    BootMode = NAND
    Starting NAND Copy...
    Valid magicnum, 0xA1ACED66, found in block 0x00000019.
       DONE
    Jumping to entry point at 0x81080000.


    U-Boot 2009.03-svn ( 4鏈?25 2011 - 15:43:32)  2011-04-22

    I2C:   ready
    DRAM: 256 MB
    NAND:  NAND device: Manufacturer ID: 0x2c, Chip ID: 0x48 (Micron NAND 2GiB 3,3V 8-bit)
    2048 MiB
    *** Warning - bad CRC or NAND, using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Ethernet PHY: GENERIC @ 0x01
    Hit any key to stop autoboot:  0

    NAND read: device 0 offset 0x2400000, size 0x100
     256 bytes read: OK

    NAND read: device 0 offset 0xb400000, size 0xa00000
     10485760 bytes read: OK
    check cramfs crc ok 0x76100162

    Loading from NAND 2GiB 3,3V 8-bit, offset 0xb000000
       Image Name:   Linux-2.6.18_pro500-davinci_IPNC
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1839804 Bytes =  1.8 MB
       Load Address: 80008000
       Entry Point:  80008000
    ## Booting kernel from Legacy Image at 80700000 ...
       Image Name:   Linux-2.6.18_pro500-davinci_IPNC
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1839804 Bytes =  1.8 MB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux...........................................................................................................................

    crc error

     -- System halted

    and If we set DDR PLL to 343M in uboot, the error message is different:

    DM36x initialization passed!
    TI UBL Version: 1.50 2010-11-12
    Booting Catalog Boot Loader
    BootMode = NAND
    Starting NAND Copy...
    Valid magicnum, 0xA1ACED66, found in block 0x00000019.
    DONE
    Jumping to entry point at 0x81080000.  //It's pause at here.

    The old camera board can boot from nand successfully when set DDR PLL to 343M. And our hardware engineer is very sure that have no different between the old and new board in nand and DDR drawing.

    so, we are meeting a urgent problem.  Anyboady can give me some advice about this problem?

    Thanks a lot.


  • Hi,

         Thanks for everyone who be care for the problem!

         We had find the reason of the problem. We make a mistake to using the resistance of related to DDR.

        Make mistake to use 49.9K Ohm, it must be using 49.9Ohm.

        Thanks a lot!