This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM64: SKAM64 -A

 Part Number: SK-AM64

Hi , 

I was trying to configure the internal 12 bit ADC which is there in the skam64 , for the external analog data as the input , in the technical reference manual 8 analog input pins are mentioned for the ADC , but when i did check in the schematic , it seems that none of the input pins are available on board for the external connection ,also in the schematic , all the pins are grounded.

I want to use this ADC with the external input ,is there a way to provide the external input ?

Regards,

Shruti Gupta