This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs v3.1 and tms320c6713

Hi all,

I am working with tms320c6713 and ccsv3.1...............i am able to run programs and get the output on this kit ..........but i face a problem........I am giving the input (recorded signal)through LINE IN............My output is viewed through LEDs..........When i give one signal i should get output'10' in the LED or else for the second signal output in the LED should be '5'...............But in both cases i am getting 10 as output..............the same model works fine in simulation in case of both inputs..........pls help

 

mridula

  • Mridula,

    Try running on the kit the exact same way you run on the simulator, and see if the results are different. With the same input data in both cases, the output data should be the same, too.

    Regards,
    RandyP