This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3LX: XDS110: Troubleshooting

Part Number: TDA3LX

Hi Experts,

We need your assistance.

We are using an XDS110 debugger and when we try to connect in CCS there are such errors and we can't connect. What could this be caused by?

Cortex_M4_IPU1_C1: GEL Output: --->>> TDA3xx Cortex M4 Startup Sequence In Progress... <<<---
Cortex_M4_IPU1_C1: GEL Output: --->>> TDA3xx Cortex M4 Startup Sequence DONE! <<<---
ARP32_EVE_1: GEL Output: --->>> Configuring EVE Memory Map <<<---
ARP32_EVE_1: GEL Output: --->>> EVE Memory Map Done! <<<---
Cortex_M4_IPU1_C0: Trouble Setting Breakpoint with the Action "Process CIO" at 0x800c22a2: (Error -1066 @ 0x800C22A2) Unable to set/clear requested breakpoint. Verify that the breakpoint address is invalid memory. (Emulation package 9.10.0.00080) 
Cortex_M4_IPU1_C0: Breakpoint Manager: Retrying with a AET breakpoint
Cortex_M4_IPU1_C0: Breakpoint Manager: Error enabling this function: Address exceeds the allowed range
Cortex_M4_IPU1_C0: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x800c7060: (Error -1066 @ 0x800C7060) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.10.0.00080) 
Cortex_M4_IPU1_C0: Breakpoint Manager: Retrying with a AET breakpoint
Cortex_M4_IPU1_C0: Breakpoint Manager: Error enabling this function: Address exceeds the allowed range
Cortex_M4_IPU1_C0: Trouble Setting Breakpoint with the Action "Remain Halted" at 0x80060908: (Error -1066 @ 0x80060908) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.10.0.00080) 
Cortex_M4_IPU1_C0: Breakpoint Manager: Retrying with a AET breakpoint
Cortex_M4_IPU1_C0: Breakpoint Manager: Error enabling this function: Address exceeds the allowed range

Thank you in advance.

Best regards,

Jonathan