Other Parts Discussed in Thread: ADS1606, OMAP-L138
I have a tmdxoskl138 EVM which is the L138/C6748 development kit that I would like to test the ads1606 evm with. Does the 5-6K interface module allow me to connect the two evm modules together?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Randy,
You can see in the document http://www.ti.com/litv/pdf/slau104a that:
"The 5−6K Interface Board provides a complete system development platform using evaluation modules from the Data Acquisition Products Group. This board passes signals from TMS320C5000 and TMS320C6000 Interface (SPRA711)"Daughtercard connectors defined in the TMS320 Cross-Platform daughtercardDSK platforms featuring the 80-pin"
The OMAP-L138 EVM does not have the 80-pin conector, so you would need to do a lot of adaptations. For the OMAP-L138 schematics, please click on the links below. Click on the Kit Contents or Tech Specs tab, and scroll down to Hardware Documents and Design Files
http://www.logicpd.com/products/development-kits/zoom-omap-l138-experimenter-kit
http://www.logicpd.com/products/development-kits/zoom-omap-l138-evm-development-kit
http://www.logicpd.com/products/system-modules/texas-instruments-omap-l138-som-m1
You do not need to have a board to get the schematics, just to have an account at the LogicPD website.