Hi,
I'm wondering if there is a H.264 encoder codec with Linux EZ.
If so, does it take the fully advantage of HDVICP 2? And whether is it a evaluation version?
Thank u!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The EZSDK has an H264 codec built into the media controller firmware. It isn't a stand alone file as it was before that would get integrated into a codec server. I believe it uses the HDVICP2 for which there is no openly available documentation (so you can't make use of it directly). The codecs are royalty free full versions as I understand so they aren't evaluation.
Ralph
Documentation can be found under :
ti-ezsdk_dm816x-evm_5_01_01_80\omx_05_01_01_80\packages\ti\omx\docs