Part Number: PROCESSOR-SDK-AM62X
Hi,
Here I am discussing a known issue: Device Id Register is missing for AM62x-SK
Baseline:
Processor SDK 08.03.00.19
Problem Statement:
As device Id register address is not defined in AM62x TRM.
- What is the base address to read device id register ?
- an we read via omapconf or devmem utils ?

Solution:
For Windows Setup:
- Please refer page to make setup
- Connect the device (AM62x) to windows PC running CCS using XDS110
- Go to View => Memory Browser
- Enter Register address 0x43000014. you should get the device Id

For Linux Setup:
- Downloaded tisdk-default-image-am62xx-evm.wic.xz from https://www.ti.com/tool/download/PROCESSOR-SDK-LINUX-AM62X/08.03.00.19
- Set SD card boot mode referring https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/08_03_00_19/exports/docs/linux/How_to_Guides/Hardware_Setup_with_CCS/AM62x_EVM_Hardware_Setup.html
- Create SD card using "1.1.3.2. Create SD Card using balenaEtcher" mentioned in https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/08_03_00_19/exports/docs/linux/Overview/Processor_SDK_Linux_create_SD_card.html
- Insert card and power cycle the board
- Then run below commands and get device-id
========================================================================================
========================================================================================
Best Regards
Ashwani