This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6747 McAsp Transmit/Receive Sync via SIO Module

I'm trying to interface the C6747 McAsp to a multi-channel A/D device (AD7490) using 2 serializers in burst mode. One serializer is used to write/initialize the AD7490 and the other is for reading the output of the AD7490.  I'm using the DSP/BIOS SIO module commands such as SIO_issue, SIO_reclaim, etc. I'm able to initialize the device and read the data but I need to synchronize the reading of the buffer with the transmit operation that is initializing the AD7490 such that the A/D data channels will arrive in the input buffer in a fixed order.  How do I go about synchronizing the transmit and receive operations using the DSP/BIOS SIO module?

Thanks,

Tim